+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Miniature Electromagnetic Relays

(3 647)

The function performed by electromagnetic relays is trivial but extremely important. Relays are electromechanically operated switches that use a low level control signal to switch a much higher voltage or current supply. They can also perform the opposite function, e.g., turn on a lamp on the panel, signalling the flow of high current in the controlled circuit.

An electromagnetic relay consists of a coil and contacts and uses an electromagnet to close or open the contacts. In other words: applying a voltage to the coil closes or opens the circuit (or several circuits, depending on the pin configuration).

Electromagnetic relays are known in automation for many decades. Their design still undergoes some modifications, but their advantages and limitations remain the same. The main advantage is the isolation of the control and controlled circuits. This gives electromagnetic relays a certain advantage over alternatives such as electronic circuits based on semiconductors (transistors). This feature is particularly appreciated in the consumer electronics and white goods industry, where the safety of users is important, even in the event of improper handling. In many cases relays also have the advantage of being simple in design and easy to use in electronic/electrical circuits. Replacing relays in your vehicle, control unit, and machinery is not a problem. Many relays are designed for quick assembly and disassembly, use dedicated sockets, and are produced in standard formats, which facilitates the work of mechanics, maintenance technicians, etc. Unfortunately, relays also have their drawbacks - although the control currents are low, they can be considered substantial (tens or hundreds of milliamps) for energy-saving applications. As they are mechanical components, they have a certain degree of failure and are not able to match their semiconductor counterparts when it comes to the switching frequency.

Let's take a look at the basic features of electromagnetic relays that should be kept in mind when selecting the right components for your applications or when looking for a replacement for a damaged component.

Relay Contact Configuration

The first aspect is the configuration of the contacts. The most important abbreviations are: NO (normally open) and NC (normally closed). This means that the relay-controlled circuit can be normally closed or normally open, depending on the needs. Obviously, in the case when the purpose of the relay is to temporarily interrupt the supply - a relay that opens the circuit when triggered shall be used. This results in less wear on the relay, which will not consume energy during normal operation of the device.

Apart from the abbreviations NO and NC, the most common contact configurations are:

SPST (Single Pole Single Throw) - the simplest switch used to make or break the connection between each input contact and its designated output contact.

SPDT (Single Pole Double Throw) – this switch contains one input, which can switch between two outputs, i.e., can connect to and switch between two outputs. When there is no voltage applied to the coil one circuit “receives” current, the other one does not.

DPST (Double Pole Single Throw) is a switch that has 2 inputs and 2 outputs. A single control signal activates two independent circuits. Such a relay can be used for simultaneously controlling, e.g. a load and an indicator light.

DPDT (Double Pole Double Throw) - two input contacts that can be in one of two positions, i.e. connected to one set of output contacts.

TME customers looking for more pin pitch options can use the technical drawings visible when hovering the mouse over the information icon in the "Contact Configuration" field (this is one of the filters visible at the top of the page).

Basic parameters of electromagnetic relays

In addition to the contact configuration, the important parameters of relays mainly concern their electrical characteristics. A distinction should be made here:

Relay version - this specifies the general characteristics of the element (e.g., whether it is used to control signals or is resistant to high inrush currents of inductive loads such as motors). There is also a division into bistable and monostable versions. Bistable relays, as the name suggests, do not change their state after disconnecting the control voltage.

Nominal coil voltage - the optimum voltage that must be applied to the coil for the relay to perform its function. A voltage that is too low will be insufficient to run the circuit, while a voltage that is too high can damage the electromagnet. The distinction between AC and DC operated systems is also important here.

Maximum switching voltage - the highest potential difference that can occur in the controlled circuit. Exceeding this value may result not only in damage to the relay, but also in electrical breakdown and failure of the controller (this in turn poses a risk to the health and life of the operators!). The same applies to the Maximum load capacity of AC contacts.

Mounting, size, and pitch - relays usually have a characteristic pin pitch, which prevents their incorrect mounting. For PCB mounted components, the output layout is usually compatible with typical pitches (2.54 mm, 5.08 mm, etc.). There are also surface-mount (SMT) relays. However, in the case of industrial solutions, we most often encounter base-mounted elements - this makes it easier to replace the relay and minimises the resistance of the connections.

Coil resistance - this parameter allows you to determine the energy consumption to be expected when using the component. It also makes it possible to estimate whether the relay will not overheat.

Products: 3 647

Warehouse:

TME
All
Page 1
NEW
RSM822P-2112-85-S012 | Relay: electromagnetic; Ucoil: 12VDC; DPDT; 2A; 1A/125VAC; 2A/30VDC
Relay: electromagnetic; Ucoil: 12VDC; DPDT; 2A; 1A/125VAC; 2A/30VDC
Manufacturer part number: RSM822P-2112-85-S012
Manufacturer: RELPOL
Net price for quantities from 1 pcs - 1.74 USDGross price for quantities from 1 pcs - 1.74 USD
Net price for quantities from 5 pcs - 1.57 USDGross price for quantities from 5 pcs - 1.57 USD
Net price for quantities from 20 pcs - 1.42 USDGross price for quantities from 20 pcs - 1.42 USD
Net price for quantities from 100 pcs - 1.14 USDGross price for quantities from 100 pcs - 1.14 USD
Net price for quantities from 500 pcs - 1.02 USDGross price for quantities from 500 pcs - 1.02 USD
542 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
NEW
OW5669.16/460/61 | Relay: electromagnetic; Ucoil: 12VDC; SPST-NO + SPST-NC; THT; 210Ω
Relay: electromagnetic; Ucoil: 12VDC; SPST-NO + SPST-NC; THT; 210Ω
Manufacturer part number: OW5669.16/460/61
Manufacturer: DOLD
Net price for quantities from 1 pcs - 23.41 USDGross price for quantities from 1 pcs - 23.41 USD
Net price for quantities from 5 pcs - 22.13 USDGross price for quantities from 5 pcs - 22.13 USD
Net price for quantities from 10 pcs - 20.73 USDGross price for quantities from 10 pcs - 20.73 USD
Net price for quantities from 20 pcs - 19.45 USDGross price for quantities from 20 pcs - 19.45 USD
0 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
NEW
AZ9371-1A-12DE | Relay: electromagnetic; Ucoil: 12VDC; SPST-NO; 5A; 5A/250VAC; PCB
Relay: electromagnetic; Ucoil: 12VDC; SPST-NO; 5A; 5A/250VAC; PCB
Manufacturer part number: AZ9371-1A-12DE
Manufacturer: ZETTLER
Net price for quantities from 1 pcs - 0.96 USDGross price for quantities from 1 pcs - 0.96 USD
Net price for quantities from 5 pcs - 0.87 USDGross price for quantities from 5 pcs - 0.87 USD
Net price for quantities from 25 pcs - 0.82 USDGross price for quantities from 25 pcs - 0.82 USD
Net price for quantities from 50 pcs - 0.77 USDGross price for quantities from 50 pcs - 0.77 USD
Net price for quantities from 250 pcs - 0.69 USDGross price for quantities from 250 pcs - 0.69 USD
960 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
NEW
8693260000 | Relay: electromagnetic; Ucoil: 24VDC; SPDT; Icontacts max: 16A; RCL
Relay: electromagnetic; Ucoil: 24VDC; SPDT; Icontacts max: 16A; RCL
Manufacturer part number: 8693260000
Manufacturer: WEIDMÜLLER
Net price for quantities from 1 pcs - 5.56 USDGross price for quantities from 1 pcs - 5.56 USD
Net price for quantities from 10 pcs - 5.22 USDGross price for quantities from 10 pcs - 5.22 USD
Net price for quantities from 20 pcs - 4.88 USDGross price for quantities from 20 pcs - 4.88 USD
Net price for quantities from 40 pcs - 4.55 USDGross price for quantities from 40 pcs - 4.55 USD
0 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
NEW
3052320000 | Relay: electromagnetic; Ucoil: 24VAC; SPDT; Icontacts max: 16A; CRI
Relay: electromagnetic; Ucoil: 24VAC; SPDT; Icontacts max: 16A; CRI
Manufacturer part number: 3052320000
Manufacturer: WEIDMÜLLER
Net price for quantities from 1 pcs - 6.15 USDGross price for quantities from 1 pcs - 6.15 USD
Net price for quantities from 10 pcs - 5.77 USDGross price for quantities from 10 pcs - 5.77 USD
Net price for quantities from 20 pcs - 5.39 USDGross price for quantities from 20 pcs - 5.39 USD
Net price for quantities from 50 pcs - 5.00 USDGross price for quantities from 50 pcs - 5.00 USD
5 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
NEW
RSM822P-2112-85-S024 | Relay: electromagnetic; Ucoil: 24VDC; DPDT; 2A; 1A/125VAC; 2A/30VDC
Relay: electromagnetic; Ucoil: 24VDC; DPDT; 2A; 1A/125VAC; 2A/30VDC
Manufacturer part number: RSM822P-2112-85-S024
Manufacturer: RELPOL
Net price for quantities from 1 pcs - 1.91 USDGross price for quantities from 1 pcs - 1.91 USD
Net price for quantities from 5 pcs - 1.74 USDGross price for quantities from 5 pcs - 1.74 USD
Net price for quantities from 20 pcs - 1.56 USDGross price for quantities from 20 pcs - 1.56 USD
Net price for quantities from 100 pcs - 1.26 USDGross price for quantities from 100 pcs - 1.26 USD
Net price for quantities from 500 pcs - 1.15 USDGross price for quantities from 500 pcs - 1.15 USD
58 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
NEW
AZSR250-2AE-24D | Relay: electromagnetic power; Ucoil: 24VDC; SPST-NO; 50A; PCB
Relay: electromagnetic power; Ucoil: 24VDC; SPST-NO; 50A; PCB
Manufacturer part number: AZSR250-2AE-24D
Manufacturer: ZETTLER
Net price for quantities from 100 pcs - 10.92 USDGross price for quantities from 100 pcs - 10.92 USD
0 in TME stock
No. of pieces (Multiplicity: 100)
Minimum order quantity: 100.
Multiplicity: 100.
NEW
Relay: electromagnetic; Ucoil: 5VDC; SPST-NO; 10A; 5A/250VAC; THT
Manufacturer part number: HF33F/005-HSL3
Manufacturer: HONGFA RELAY
Net price for quantities from 1000 pcs - 0.62 USDGross price for quantities from 1000 pcs - 0.62 USD
0 in TME stock
No. of pieces (Multiplicity: 100)
Minimum order quantity: 1 000.
Multiplicity: 100.
NEW
Relay: electromagnetic; Ucoil: 24VDC; 3PST-NO + SPST-NC; 8A; PCB
Manufacturer part number: 3-1415353-1
Manufacturer: TE Connectivity
Net price for quantities from 1 pcs - 42.04 USDGross price for quantities from 1 pcs - 42.04 USD
Net price for quantities from 5 pcs - 39.83 USDGross price for quantities from 5 pcs - 39.83 USD
Net price for quantities from 20 pcs - 37.62 USDGross price for quantities from 20 pcs - 37.62 USD
Net price for quantities from 100 pcs - 32.15 USDGross price for quantities from 100 pcs - 32.15 USD
0 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
NEW
Relay: electromagnetic; Ucoil: 12VDC; SPDT; 6A; 6A/250VAC; 6A/30VDC
Manufacturer part number: HF41F/12-Z8ST
Manufacturer: HONGFA RELAY
Net price for quantities from 2000 pcs - 1.71 USDGross price for quantities from 2000 pcs - 1.71 USD
0 in TME stock
No. of pieces (Multiplicity: 100)
Minimum order quantity: 2 000.
Multiplicity: 100.
NEW
Relay: electromagnetic; Ucoil: 24VDC; SPST-NO; 10A; 10A/250VAC; THT
Manufacturer part number: HF115F-H/024-1H1A
Manufacturer: HONGFA RELAY
Net price for quantities from 1000 pcs - 1.57 USDGross price for quantities from 1000 pcs - 1.57 USD
0 in TME stock
No. of pieces (Multiplicity: 1 000)
Minimum order quantity: 1 000.
Multiplicity: 1 000.
NEW
Relay: electromagnetic; Ucoil: 9VDC; SPST-NO; 16A/250VAC; HF152F
Manufacturer part number: HF152F/009-1HT
Manufacturer: HONGFA RELAY
Net price for quantities from 1000 pcs - 1.22 USDGross price for quantities from 1000 pcs - 1.22 USD
0 in TME stock
No. of pieces (Multiplicity: 1 000)
Minimum order quantity: 1 000.
Multiplicity: 1 000.
NEW
Relay: electromagnetic; Ucoil: 3VDC; DPDT; Icontacts max: 1A; SMD
Manufacturer part number: TXS2SA3J
Manufacturer: PANASONIC
Net price for quantities from 1000 pcs - 2.67 USDGross price for quantities from 1000 pcs - 2.67 USD
0 in TME stock
No. of pieces (Multiplicity: 1 000)
Minimum order quantity: 1 000.
Multiplicity: 1 000.
NEW
Relay: electromagnetic; Ucoil: 12VDC; DPDT; 0.3A/125VAC; 1A/30VDC
Manufacturer part number: HFD4/12-LSR(825)
Manufacturer: HONGFA RELAY
Net price for quantities from 3600 pcs - 1.26 USDGross price for quantities from 3600 pcs - 1.26 USD
0 in TME stock
No. of pieces (Multiplicity: 900)
Minimum order quantity: 3 600.
Multiplicity: 900.
NEW
Relay: electromagnetic; Ucoil: 12VDC; SPST-NO; 10A; 5A/250VAC; THT
Manufacturer part number: HF32F/012-HS3
Manufacturer: HONGFA RELAY
Net price for quantities from 1000 pcs - 0.41 USDGross price for quantities from 1000 pcs - 0.41 USD
0 in TME stock
No. of pieces (Multiplicity: 100)
Minimum order quantity: 1 000.
Multiplicity: 100.
NEW
Relay: electromagnetic
Manufacturer part number: HF115F-L/5-2ZS4L2TF
Manufacturer: HONGFA RELAY
Net price for quantities from 500 pcs - 3.16 USDGross price for quantities from 500 pcs - 3.16 USD
0 in TME stock
No. of pieces (Multiplicity: 500)
Minimum order quantity: 500.
Multiplicity: 500.
NEW
Relay: electromagnetic; Ucoil: 12VDC; SPST-NO; 16A; 16A/250VAC; THT
Manufacturer part number: HF115F-I/012-1H3A(335)
Manufacturer: HONGFA RELAY
Net price for quantities from 1000 pcs - 1.59 USDGross price for quantities from 1000 pcs - 1.59 USD
0 in TME stock
No. of pieces (Multiplicity: 1 000)
Minimum order quantity: 1 000.
Multiplicity: 1 000.
NEW
Relay: electromagnetic; Ucoil: 5VDC; SPDT; 16A; 16A/250VAC; HF115FK
Manufacturer part number: HF115FK/5-Z3T
Manufacturer: HONGFA RELAY
Net price for quantities from 500 pcs - 1.40 USDGross price for quantities from 500 pcs - 1.40 USD
0 in TME stock
No. of pieces (Multiplicity: 500)
Minimum order quantity: 500.
Multiplicity: 500.
NEW
Relay: electromagnetic; Ucoil: 6VDC; SPST-NO; 10A/250VAC; HF118F
Manufacturer part number: HF118F/006-1HS1(136)
Manufacturer: HONGFA RELAY
Net price for quantities from 1000 pcs - 1.11 USDGross price for quantities from 1000 pcs - 1.11 USD
0 in TME stock
No. of pieces (Multiplicity: 1 000)
Minimum order quantity: 1 000.
Multiplicity: 1 000.
NEW
Relay: electromagnetic; Ucoil: 12VDC; DPDT; 8A; 8A/250VAC; HF115F
Manufacturer part number: HF115F/012-2ZS4BF
Manufacturer: HONGFA RELAY
Net price for quantities from 500 pcs - 1.71 USDGross price for quantities from 500 pcs - 1.71 USD
0 in TME stock
No. of pieces (Multiplicity: 500)
Minimum order quantity: 500.
Multiplicity: 500.