+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Resonators and Generators

(211)

What are resonators, resistors, and cristal oscillators?

A quartz resonator is an electronic device, which is used to keep track of time with high precision. This accuracy is due to the electric pulses generated at equal intervals. This phenomenon is referred to as fixed clock rate. Resonators are used, among others in microcontroller development boards, computers, TV remote controls, toys, watches and many other commonly used electronic equipment. Quartz resonators are also commonly known as quartz crystals, but you can also meet terms such as quartz resistor or quartz oscillator.

Resonator types

There are several types of resonators. The most popular of these are quartz resonators, but there are alsoceramic resonators, and the increasingly popular silicon resonators. The quartz resonators used in watches are a special variety of resonators (oscillators).

Quartz crystal resonators. made of a precisely cut quartz crystal, i.e. silicon dioxide (SiO2), have two leads. They are attached to metal electrodes. The different natural frequency of the resonator is achieved by the different shape and size of the quartz used. Ceramic resonators have a similar structure, but their main element is a piezoelectric material other than quartz.

Quartz resonators use the piezoelectric effect, which is the ability of certain materials to generate an electric charge in response to applied mechanical stress (the ends of the crystal become electrically charged). Piezoelectric material also exhibits the reverse piezoelectric effect. When a voltage difference is applied to its ends, it deforms. The quartz resonator connected to an electronic circuit causes it to vibrate; by supplying energy to the circuit, it generates a mechanical resonance with a frequency equal to the natural frequency of the used quartz crystal. The most common type of electronic oscillator is the Pierce oscillator.Sometimes you can find ready-made modules in the form of pulse generators. They have on-board electronics and usually 4 leads, which are responsible for ground and power supply, pulse output and control input.

Quartz resonator properties - accuracy and frequency

he accuracy of quartz resonators is determined by a unit called PPM (parts per million). For example, 1% accuracy is equal to 10 000 PPM. It is particularly important, among other things, in high quality watches so that these do not lose or gain a few seconds per day. Quartz resonators have the highest accuracy with an average of several tens of PPM, which in practice means a range of roughly 3 to 100 PPM. Currently manufactured ceramic resonators have very similar stability, starting at around 10 PPM, while quartz resonators used in watches do not exceed 20 PPM.

Please note that the accuracy and stability of the pulses generated by crystal resonator are highly dependent on temperature. Thus, constant temperature crystal oscillators are available; this is possible thanks to an additional electronic circuit. It is interesting to note that the frequency of the pulses generated by a resonator can even be affected by its spatial orientation relative to the gravity vector, as the force of the Earth's attraction can to some extent alter he frequency of natural vibrations of the crystal.

Of course, in addition to accuracy, the frequency is equally important with quartz resonators. This value can range from tens of kilohertz[kHz] to tens of megahertz [MHz]. The quartz resonators used in watches could be the most interesting here, as they will have a frequency of 32 768 kHz in virtually every case. This is due by the fact that when you divide this value by two to the power of fifteen, you get a pulse once per second, the time base of an analogue clock.

Quartz resonator parameters

The frequency of the resonator is usually stamped on the package. Unfortunately, like most devices, quartz resonators can change their frequency characteristics to some degree over time due to aging.

Selection of quartz crystal resonators

Quartz crystal oscillators, like virtually any other electronic component, are available in THT or SMD packages.

When choosing a quartz resonator, the pitch of the resonator, affecting mechanical compatibility, should be taken into account. The term is used to describe the distance between the leads of electronic components, e.g., integrated circuits or terminal blocks. The standard pitches for quartz resonators are 0.7mm, 1.1mm, 2.54mm, 4.88mm, and 5.1mm.

The most common package types for quartz crystal oscillators are cylindrical packages (HC-49, HC-49-S, HC-49/U, TC26, and TC38) which are THT (through-hole mounting) packages, and HC-49SM and HC-49SMD (SMD, surface mounting).

Attention can also be paid to a number of other parameters, such as the operating temperature, which can range from about -55°C to 150°C, power, given in milliwatts[mW] or even nanowatts [nW], but also the capacitance, which can range from about 6 pF (picofarad) to 30 F.

Products: 211

Warehouse:

TME
All
Page 1
NEW
CX3225FB16000D0FZZH1 | Crystal; 16MHz; SMD; 3.2x2.5x0.8mm; 8pF
Crystal; 16MHz; SMD; 3.2x2.5x0.8mm; 8pF
Manufacturer part number: CX3225FB16000D0FZZH1
Manufacturer: KYOCERA AVX
Net price for quantities from 1 pcs - 0.24 USDGross price for quantities from 1 pcs - 0.24 USD
Net price for quantities from 10 pcs - 0.22 USDGross price for quantities from 10 pcs - 0.22 USD
Net price for quantities from 50 pcs - 0.20 USDGross price for quantities from 50 pcs - 0.20 USD
Net price for quantities from 100 pcs - 0.19 USDGross price for quantities from 100 pcs - 0.19 USD
Net price for quantities from 500 pcs - 0.17 USDGross price for quantities from 500 pcs - 0.17 USD
Net price for quantities from 1500 pcs - 0.17 USDGross price for quantities from 1500 pcs - 0.17 USD
Net price for quantities from 3000 pcs - 0.15 USDGross price for quantities from 3000 pcs - 0.15 USD
2048 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
NEW
WTL1X80739BEL | Resonator: quartz; 32.768kHz; SMD; 3.2x1.5x0.75mm; ±20ppm
Resonator: quartz; 32.768kHz; SMD; 3.2x1.5x0.75mm; ±20ppm
Manufacturer part number: WTL1X80739BEL
Manufacturer: WTL
Net price for quantities from 1 pcs - 0.38 USDGross price for quantities from 1 pcs - 0.38 USD
Net price for quantities from 10 pcs - 0.28 USDGross price for quantities from 10 pcs - 0.28 USD
Net price for quantities from 100 pcs - 0.22 USDGross price for quantities from 100 pcs - 0.22 USD
Net price for quantities from 500 pcs - 0.21 USDGross price for quantities from 500 pcs - 0.21 USD
Net price for quantities from 1000 pcs - 0.20 USDGross price for quantities from 1000 pcs - 0.20 USD
Net price for quantities from 3000 pcs - 0.20 USDGross price for quantities from 3000 pcs - 0.20 USD
Net price for quantities from 6000 pcs - 0.19 USDGross price for quantities from 6000 pcs - 0.19 USD
Net price for quantities from 9000 pcs - 0.18 USDGross price for quantities from 9000 pcs - 0.18 USD
Net price for quantities from 15000 pcs - 0.18 USDGross price for quantities from 15000 pcs - 0.18 USD
Net price for quantities from 30000 pcs - 0.18 USDGross price for quantities from 30000 pcs - 0.18 USD
11190 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
NEW
CX3225FB24000F0FZZH1 | Crystal; 24MHz; SMD; 3.2x2.5x0.8mm; 10pF
Crystal; 24MHz; SMD; 3.2x2.5x0.8mm; 10pF
Manufacturer part number: CX3225FB24000F0FZZH1
Manufacturer: KYOCERA AVX
Net price for quantities from 1 pcs - 0.25 USDGross price for quantities from 1 pcs - 0.25 USD
Net price for quantities from 10 pcs - 0.22 USDGross price for quantities from 10 pcs - 0.22 USD
Net price for quantities from 25 pcs - 0.21 USDGross price for quantities from 25 pcs - 0.21 USD
Net price for quantities from 100 pcs - 0.19 USDGross price for quantities from 100 pcs - 0.19 USD
Net price for quantities from 250 pcs - 0.18 USDGross price for quantities from 250 pcs - 0.18 USD
Net price for quantities from 500 pcs - 0.17 USDGross price for quantities from 500 pcs - 0.17 USD
Net price for quantities from 1500 pcs - 0.16 USDGross price for quantities from 1500 pcs - 0.16 USD
Net price for quantities from 3000 pcs - 0.15 USDGross price for quantities from 3000 pcs - 0.15 USD
0 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
NEW
CX3225FB16000F0FZZH1 | Crystal; 16MHz; SMD; 3.2x2.5x0.8mm; 10pF
Crystal; 16MHz; SMD; 3.2x2.5x0.8mm; 10pF
Manufacturer part number: CX3225FB16000F0FZZH1
Manufacturer: KYOCERA AVX
Net price for quantities from 1 pcs - 0.33 USDGross price for quantities from 1 pcs - 0.33 USD
Net price for quantities from 10 pcs - 0.29 USDGross price for quantities from 10 pcs - 0.29 USD
Net price for quantities from 25 pcs - 0.27 USDGross price for quantities from 25 pcs - 0.27 USD
Net price for quantities from 50 pcs - 0.26 USDGross price for quantities from 50 pcs - 0.26 USD
Net price for quantities from 100 pcs - 0.25 USDGross price for quantities from 100 pcs - 0.25 USD
Net price for quantities from 250 pcs - 0.24 USDGross price for quantities from 250 pcs - 0.24 USD
Net price for quantities from 500 pcs - 0.23 USDGross price for quantities from 500 pcs - 0.23 USD
Net price for quantities from 1500 pcs - 0.22 USDGross price for quantities from 1500 pcs - 0.22 USD
Net price for quantities from 3000 pcs - 0.20 USDGross price for quantities from 3000 pcs - 0.20 USD
1724 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
NEW
CX3225FB32000F0FZZH1 | Crystal; 32MHz; SMD; 3.2x2.5x0.8mm; 10pF
Crystal; 32MHz; SMD; 3.2x2.5x0.8mm; 10pF
Manufacturer part number: CX3225FB32000F0FZZH1
Manufacturer: KYOCERA AVX
Net price for quantities from 1 pcs - 0.24 USDGross price for quantities from 1 pcs - 0.24 USD
Net price for quantities from 10 pcs - 0.21 USDGross price for quantities from 10 pcs - 0.21 USD
Net price for quantities from 25 pcs - 0.20 USDGross price for quantities from 25 pcs - 0.20 USD
Net price for quantities from 50 pcs - 0.19 USDGross price for quantities from 50 pcs - 0.19 USD
Net price for quantities from 100 pcs - 0.18 USDGross price for quantities from 100 pcs - 0.18 USD
Net price for quantities from 250 pcs - 0.17 USDGross price for quantities from 250 pcs - 0.17 USD
Net price for quantities from 500 pcs - 0.17 USDGross price for quantities from 500 pcs - 0.17 USD
Net price for quantities from 1500 pcs - 0.16 USDGross price for quantities from 1500 pcs - 0.16 USD
Net price for quantities from 3000 pcs - 0.15 USDGross price for quantities from 3000 pcs - 0.15 USD
2851 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
NEW
CX3225FB40000F0FZZH1 | Crystal; 40MHz; SMD; 3.2x2.5x0.8mm; 10pF
Crystal; 40MHz; SMD; 3.2x2.5x0.8mm; 10pF
Manufacturer part number: CX3225FB40000F0FZZH1
Manufacturer: KYOCERA AVX
Net price for quantities from 1 pcs - 0.24 USDGross price for quantities from 1 pcs - 0.24 USD
Net price for quantities from 10 pcs - 0.21 USDGross price for quantities from 10 pcs - 0.21 USD
Net price for quantities from 25 pcs - 0.20 USDGross price for quantities from 25 pcs - 0.20 USD
Net price for quantities from 50 pcs - 0.19 USDGross price for quantities from 50 pcs - 0.19 USD
Net price for quantities from 100 pcs - 0.18 USDGross price for quantities from 100 pcs - 0.18 USD
Net price for quantities from 250 pcs - 0.17 USDGross price for quantities from 250 pcs - 0.17 USD
Net price for quantities from 500 pcs - 0.17 USDGross price for quantities from 500 pcs - 0.17 USD
Net price for quantities from 1500 pcs - 0.16 USDGross price for quantities from 1500 pcs - 0.16 USD
Net price for quantities from 3000 pcs - 0.15 USDGross price for quantities from 3000 pcs - 0.15 USD
2878 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
NEW
CX2016FB32000D0FZZH1 | Crystal; 32MHz; SMD; 2x1.6x0.55mm; 8pF
Crystal; 32MHz; SMD; 2x1.6x0.55mm; 8pF
Manufacturer part number: CX2016FB32000D0FZZH1
Manufacturer: KYOCERA AVX
Net price for quantities from 1 pcs - 0.24 USDGross price for quantities from 1 pcs - 0.24 USD
Net price for quantities from 10 pcs - 0.22 USDGross price for quantities from 10 pcs - 0.22 USD
Net price for quantities from 50 pcs - 0.20 USDGross price for quantities from 50 pcs - 0.20 USD
Net price for quantities from 100 pcs - 0.19 USDGross price for quantities from 100 pcs - 0.19 USD
Net price for quantities from 500 pcs - 0.17 USDGross price for quantities from 500 pcs - 0.17 USD
Net price for quantities from 1500 pcs - 0.17 USDGross price for quantities from 1500 pcs - 0.17 USD
Net price for quantities from 3000 pcs - 0.15 USDGross price for quantities from 3000 pcs - 0.15 USD
2678 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
NEW
CX3225FB25000D0FZZH1 | Crystal; 25MHz; SMD; 3.2x2.5x0.8mm; 8pF
Crystal; 25MHz; SMD; 3.2x2.5x0.8mm; 8pF
Manufacturer part number: CX3225FB25000D0FZZH1
Manufacturer: KYOCERA AVX
Net price for quantities from 1 pcs - 0.24 USDGross price for quantities from 1 pcs - 0.24 USD
Net price for quantities from 10 pcs - 0.21 USDGross price for quantities from 10 pcs - 0.21 USD
Net price for quantities from 25 pcs - 0.20 USDGross price for quantities from 25 pcs - 0.20 USD
Net price for quantities from 50 pcs - 0.19 USDGross price for quantities from 50 pcs - 0.19 USD
Net price for quantities from 100 pcs - 0.18 USDGross price for quantities from 100 pcs - 0.18 USD
Net price for quantities from 250 pcs - 0.17 USDGross price for quantities from 250 pcs - 0.17 USD
Net price for quantities from 500 pcs - 0.17 USDGross price for quantities from 500 pcs - 0.17 USD
Net price for quantities from 1500 pcs - 0.16 USDGross price for quantities from 1500 pcs - 0.16 USD
Net price for quantities from 3000 pcs - 0.15 USDGross price for quantities from 3000 pcs - 0.15 USD
2960 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
NEW
CX2016FB24000D0FZZH1 | Crystal; 24MHz; SMD; 2x1.6x0.55mm; 8pF
Crystal; 24MHz; SMD; 2x1.6x0.55mm; 8pF
Manufacturer part number: CX2016FB24000D0FZZH1
Manufacturer: KYOCERA AVX
Net price for quantities from 1 pcs - 0.24 USDGross price for quantities from 1 pcs - 0.24 USD
Net price for quantities from 10 pcs - 0.22 USDGross price for quantities from 10 pcs - 0.22 USD
Net price for quantities from 50 pcs - 0.20 USDGross price for quantities from 50 pcs - 0.20 USD
Net price for quantities from 100 pcs - 0.19 USDGross price for quantities from 100 pcs - 0.19 USD
Net price for quantities from 500 pcs - 0.17 USDGross price for quantities from 500 pcs - 0.17 USD
Net price for quantities from 1500 pcs - 0.17 USDGross price for quantities from 1500 pcs - 0.17 USD
Net price for quantities from 3000 pcs - 0.15 USDGross price for quantities from 3000 pcs - 0.15 USD
2939 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
NEW
CX2016FB40000D0FZZH1 | Crystal; 40MHz; SMD; 2x1.6x0.55mm; 8pF
Crystal; 40MHz; SMD; 2x1.6x0.55mm; 8pF
Manufacturer part number: CX2016FB40000D0FZZH1
Manufacturer: KYOCERA AVX
Net price for quantities from 1 pcs - 0.24 USDGross price for quantities from 1 pcs - 0.24 USD
Net price for quantities from 10 pcs - 0.22 USDGross price for quantities from 10 pcs - 0.22 USD
Net price for quantities from 50 pcs - 0.20 USDGross price for quantities from 50 pcs - 0.20 USD
Net price for quantities from 100 pcs - 0.19 USDGross price for quantities from 100 pcs - 0.19 USD
Net price for quantities from 500 pcs - 0.17 USDGross price for quantities from 500 pcs - 0.17 USD
Net price for quantities from 1500 pcs - 0.17 USDGross price for quantities from 1500 pcs - 0.17 USD
Net price for quantities from 3000 pcs - 0.15 USDGross price for quantities from 3000 pcs - 0.15 USD
1483 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
NEW
CX2016FB25000D0FZZH1 | Crystal; 25MHz; SMD; 2x1.6x0.55mm; 8pF
Crystal; 25MHz; SMD; 2x1.6x0.55mm; 8pF
Manufacturer part number: CX2016FB25000D0FZZH1
Manufacturer: KYOCERA AVX
Net price for quantities from 1 pcs - 0.24 USDGross price for quantities from 1 pcs - 0.24 USD
Net price for quantities from 10 pcs - 0.22 USDGross price for quantities from 10 pcs - 0.22 USD
Net price for quantities from 50 pcs - 0.20 USDGross price for quantities from 50 pcs - 0.20 USD
Net price for quantities from 100 pcs - 0.19 USDGross price for quantities from 100 pcs - 0.19 USD
Net price for quantities from 500 pcs - 0.17 USDGross price for quantities from 500 pcs - 0.17 USD
Net price for quantities from 1500 pcs - 0.17 USDGross price for quantities from 1500 pcs - 0.17 USD
Net price for quantities from 3000 pcs - 0.15 USDGross price for quantities from 3000 pcs - 0.15 USD
2977 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
NEW
CX3225FB25000F0FZZH1 | Crystal; 25MHz; SMD; 3.2x2.5x0.8mm; 10pF
Crystal; 25MHz; SMD; 3.2x2.5x0.8mm; 10pF
Manufacturer part number: CX3225FB25000F0FZZH1
Manufacturer: KYOCERA AVX
Net price for quantities from 1 pcs - 0.33 USDGross price for quantities from 1 pcs - 0.33 USD
Net price for quantities from 10 pcs - 0.29 USDGross price for quantities from 10 pcs - 0.29 USD
Net price for quantities from 25 pcs - 0.27 USDGross price for quantities from 25 pcs - 0.27 USD
Net price for quantities from 50 pcs - 0.26 USDGross price for quantities from 50 pcs - 0.26 USD
Net price for quantities from 100 pcs - 0.25 USDGross price for quantities from 100 pcs - 0.25 USD
Net price for quantities from 250 pcs - 0.23 USDGross price for quantities from 250 pcs - 0.23 USD
Net price for quantities from 500 pcs - 0.23 USDGross price for quantities from 500 pcs - 0.23 USD
Net price for quantities from 1500 pcs - 0.22 USDGross price for quantities from 1500 pcs - 0.22 USD
Net price for quantities from 3000 pcs - 0.20 USDGross price for quantities from 3000 pcs - 0.20 USD
2957 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
NEW
CX2016FB40000F0FZZH1 | Crystal; 40MHz; SMD; 2x1.6x0.55mm; 10pF
Crystal; 40MHz; SMD; 2x1.6x0.55mm; 10pF
Manufacturer part number: CX2016FB40000F0FZZH1
Manufacturer: KYOCERA AVX
Net price for quantities from 1 pcs - 0.24 USDGross price for quantities from 1 pcs - 0.24 USD
Net price for quantities from 10 pcs - 0.22 USDGross price for quantities from 10 pcs - 0.22 USD
Net price for quantities from 50 pcs - 0.20 USDGross price for quantities from 50 pcs - 0.20 USD
Net price for quantities from 100 pcs - 0.19 USDGross price for quantities from 100 pcs - 0.19 USD
Net price for quantities from 500 pcs - 0.17 USDGross price for quantities from 500 pcs - 0.17 USD
Net price for quantities from 1500 pcs - 0.17 USDGross price for quantities from 1500 pcs - 0.17 USD
Net price for quantities from 3000 pcs - 0.15 USDGross price for quantities from 3000 pcs - 0.15 USD
2971 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
NEW
CX2016FB50000D0FZZH1 | Crystal; 50MHz; SMD; 2x1.6x0.55mm; 8pF
Crystal; 50MHz; SMD; 2x1.6x0.55mm; 8pF
Manufacturer part number: CX2016FB50000D0FZZH1
Manufacturer: KYOCERA AVX
Net price for quantities from 1 pcs - 0.24 USDGross price for quantities from 1 pcs - 0.24 USD
Net price for quantities from 10 pcs - 0.22 USDGross price for quantities from 10 pcs - 0.22 USD
Net price for quantities from 50 pcs - 0.20 USDGross price for quantities from 50 pcs - 0.20 USD
Net price for quantities from 100 pcs - 0.19 USDGross price for quantities from 100 pcs - 0.19 USD
Net price for quantities from 500 pcs - 0.17 USDGross price for quantities from 500 pcs - 0.17 USD
Net price for quantities from 1500 pcs - 0.17 USDGross price for quantities from 1500 pcs - 0.17 USD
Net price for quantities from 3000 pcs - 0.15 USDGross price for quantities from 3000 pcs - 0.15 USD
2978 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
NEW
CX3225FB24000D0FZZH1 | Crystal; 24MHz; SMD; 3.2x2.5x0.8mm; 8pF
Crystal; 24MHz; SMD; 3.2x2.5x0.8mm; 8pF
Manufacturer part number: CX3225FB24000D0FZZH1
Manufacturer: KYOCERA AVX
Net price for quantities from 1 pcs - 0.33 USDGross price for quantities from 1 pcs - 0.33 USD
Net price for quantities from 10 pcs - 0.29 USDGross price for quantities from 10 pcs - 0.29 USD
Net price for quantities from 25 pcs - 0.27 USDGross price for quantities from 25 pcs - 0.27 USD
Net price for quantities from 50 pcs - 0.26 USDGross price for quantities from 50 pcs - 0.26 USD
Net price for quantities from 100 pcs - 0.25 USDGross price for quantities from 100 pcs - 0.25 USD
Net price for quantities from 250 pcs - 0.24 USDGross price for quantities from 250 pcs - 0.24 USD
Net price for quantities from 500 pcs - 0.23 USDGross price for quantities from 500 pcs - 0.23 USD
Net price for quantities from 1500 pcs - 0.22 USDGross price for quantities from 1500 pcs - 0.22 USD
Net price for quantities from 3000 pcs - 0.20 USDGross price for quantities from 3000 pcs - 0.20 USD
2970 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
NEW
CX2016FB32000F0FZZH1 | Crystal; 32MHz; SMD; 2x1.6x0.55mm; 10pF
Crystal; 32MHz; SMD; 2x1.6x0.55mm; 10pF
Manufacturer part number: CX2016FB32000F0FZZH1
Manufacturer: KYOCERA AVX
Net price for quantities from 1 pcs - 0.24 USDGross price for quantities from 1 pcs - 0.24 USD
Net price for quantities from 10 pcs - 0.22 USDGross price for quantities from 10 pcs - 0.22 USD
Net price for quantities from 50 pcs - 0.20 USDGross price for quantities from 50 pcs - 0.20 USD
Net price for quantities from 100 pcs - 0.19 USDGross price for quantities from 100 pcs - 0.19 USD
Net price for quantities from 500 pcs - 0.17 USDGross price for quantities from 500 pcs - 0.17 USD
Net price for quantities from 1500 pcs - 0.17 USDGross price for quantities from 1500 pcs - 0.17 USD
Net price for quantities from 3000 pcs - 0.15 USDGross price for quantities from 3000 pcs - 0.15 USD
2940 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
NEW
CX3225FB50000F0FZZH1 | Crystal; 50MHz; SMD; 3.2x2.5x0.8mm; 10pF
Crystal; 50MHz; SMD; 3.2x2.5x0.8mm; 10pF
Manufacturer part number: CX3225FB50000F0FZZH1
Manufacturer: KYOCERA AVX
Net price for quantities from 1 pcs - 0.24 USDGross price for quantities from 1 pcs - 0.24 USD
Net price for quantities from 10 pcs - 0.21 USDGross price for quantities from 10 pcs - 0.21 USD
Net price for quantities from 25 pcs - 0.20 USDGross price for quantities from 25 pcs - 0.20 USD
Net price for quantities from 50 pcs - 0.19 USDGross price for quantities from 50 pcs - 0.19 USD
Net price for quantities from 100 pcs - 0.18 USDGross price for quantities from 100 pcs - 0.18 USD
Net price for quantities from 250 pcs - 0.17 USDGross price for quantities from 250 pcs - 0.17 USD
Net price for quantities from 500 pcs - 0.17 USDGross price for quantities from 500 pcs - 0.17 USD
Net price for quantities from 1500 pcs - 0.16 USDGross price for quantities from 1500 pcs - 0.16 USD
Net price for quantities from 3000 pcs - 0.15 USDGross price for quantities from 3000 pcs - 0.15 USD
2990 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
NEW
CX3225FB20000D0FZZH1 | Crystal; 20MHz; SMD; 3.2x2.5x0.8mm; 8pF
Crystal; 20MHz; SMD; 3.2x2.5x0.8mm; 8pF
Manufacturer part number: CX3225FB20000D0FZZH1
Manufacturer: KYOCERA AVX
Net price for quantities from 1 pcs - 0.34 USDGross price for quantities from 1 pcs - 0.34 USD
Net price for quantities from 10 pcs - 0.29 USDGross price for quantities from 10 pcs - 0.29 USD
Net price for quantities from 50 pcs - 0.27 USDGross price for quantities from 50 pcs - 0.27 USD
Net price for quantities from 100 pcs - 0.26 USDGross price for quantities from 100 pcs - 0.26 USD
Net price for quantities from 500 pcs - 0.23 USDGross price for quantities from 500 pcs - 0.23 USD
Net price for quantities from 1500 pcs - 0.21 USDGross price for quantities from 1500 pcs - 0.21 USD
Net price for quantities from 3000 pcs - 0.20 USDGross price for quantities from 3000 pcs - 0.20 USD
Net price for quantities from 9000 pcs - 0.20 USDGross price for quantities from 9000 pcs - 0.20 USD
Net price for quantities from 12000 pcs - 0.19 USDGross price for quantities from 12000 pcs - 0.19 USD
2995 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
NEW
CX3225FB27000F0FZZH1 | Crystal; 27MHz; SMD; 3.2x2.5x0.8mm; 10pF
Crystal; 27MHz; SMD; 3.2x2.5x0.8mm; 10pF
Manufacturer part number: CX3225FB27000F0FZZH1
Manufacturer: KYOCERA AVX
Net price for quantities from 1 pcs - 0.34 USDGross price for quantities from 1 pcs - 0.34 USD
Net price for quantities from 10 pcs - 0.29 USDGross price for quantities from 10 pcs - 0.29 USD
Net price for quantities from 50 pcs - 0.27 USDGross price for quantities from 50 pcs - 0.27 USD
Net price for quantities from 100 pcs - 0.26 USDGross price for quantities from 100 pcs - 0.26 USD
Net price for quantities from 500 pcs - 0.23 USDGross price for quantities from 500 pcs - 0.23 USD
Net price for quantities from 1500 pcs - 0.21 USDGross price for quantities from 1500 pcs - 0.21 USD
Net price for quantities from 3000 pcs - 0.20 USDGross price for quantities from 3000 pcs - 0.20 USD
Net price for quantities from 9000 pcs - 0.20 USDGross price for quantities from 9000 pcs - 0.20 USD
Net price for quantities from 12000 pcs - 0.19 USDGross price for quantities from 12000 pcs - 0.19 USD
2980 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
NEW
CX3225FB20000F0FZZH1 | Crystal; 20MHz; SMD; 3.2x2.5x0.8mm; 10pF
Crystal; 20MHz; SMD; 3.2x2.5x0.8mm; 10pF
Manufacturer part number: CX3225FB20000F0FZZH1
Manufacturer: KYOCERA AVX
Net price for quantities from 1 pcs - 0.34 USDGross price for quantities from 1 pcs - 0.34 USD
Net price for quantities from 10 pcs - 0.29 USDGross price for quantities from 10 pcs - 0.29 USD
Net price for quantities from 50 pcs - 0.27 USDGross price for quantities from 50 pcs - 0.27 USD
Net price for quantities from 100 pcs - 0.26 USDGross price for quantities from 100 pcs - 0.26 USD
Net price for quantities from 500 pcs - 0.23 USDGross price for quantities from 500 pcs - 0.23 USD
Net price for quantities from 1500 pcs - 0.21 USDGross price for quantities from 1500 pcs - 0.21 USD
Net price for quantities from 3000 pcs - 0.20 USDGross price for quantities from 3000 pcs - 0.20 USD
Net price for quantities from 9000 pcs - 0.20 USDGross price for quantities from 9000 pcs - 0.20 USD
Net price for quantities from 12000 pcs - 0.19 USDGross price for quantities from 12000 pcs - 0.19 USD
2990 in TME stock