+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Strippers for wire & cable

(3)

Insulation strippers are a relatively new tool, as the first ones only appeared in the late 1990s. Today, it is difficult to imagine the work of fitters without these specialised tools; there are a variety of products on the market that are based on different technologies and tailored to your needs.

Why and how do we strip insulation from cables and wires?

The protective layer, or insulation, protects the wires from external conditions, as well as from each other. If we need to connect or install equipment, it is necessary to remove the insulation from all wires in the cable to ensure current flow once they are connected. Of course, this should be done in such a way as not to damage electrically conductive parts, which could result in dangerous consequences, e.g. ignition. When choosing how to get rid of insulation, it is necessary to consider its characteristics. There are single-layer and multi-layer insulation wires; the insulation is usually made of plastic (plastic, resins, fabrics, or non-flammable dielectrics). The end of the cable must be stripped so that its core does not become less durable and its cross-sectional area is not reduced, which will impair its electrical properties. To reduce these risks, special tools have been developed, namely strippers. The choice of stripping tools depends on the cable material, its cross-section, and its application. In our catalogue, you can filter the products according to which cables you would like to use them for.

Wire stripping pliers

Here we have a wide range of both automatic and manual products to choose from.

Automatic wire stripper

This tool is used for stripping cables and is most convenient for this application. It allows you to precisely remove a specific length of insulation. With this type of tool, you can strip the insulation of single-core cables and individual cores of multi-core cables.

Diagonal insulation strippers

Diagonal insulation strippers are a convenient and safe tool, but only when used correctly Pay attention to the direction of the blades and the applied force, otherwise it is possible to damage the conductor. When using diagonal insulation strippers, care must be taken to precisely adjust the blade to the cutting depth. Diagonal insulation strippers with precision stripping holes are also available, making them easy to use at home. Diagonal insulation strippers perform better in places difficult to reach for automatic wire strippers.

Multifunctional stripping tools

These tools are not only designed to strip the insulation off the wires but are also used as cable crimping tools to reduce the number of tools needed for the job. The lock function guarantees consistently high crimp quality and the possibility of unlocking in case of an error.

How to select an insulation stripper and use it safely

Remember not to strip the insulation too long. A wire that is stripped too long will allow the extra bare area of the conductor could become a danger to anyone who may come in contact with the wired device. Incorrectly stripped insulation can cause a short circuit or fire Practical skills play a key role in the wire stripping process. The hardest part is working with thin wires when every move matters. Optimum pressure, especially with traditional tools, is only ensured by proper practice. So, if you strip the insulation infrequently and are worried about hurting yourself or damaging the cable, it is far better to invest in advanced stripping tools from well-known brands and automatic tools. You need much less experience to use them, so the work is much easier. We should also remember to choose the tool for the cables with which we will work most often. A thin wire stripper is a completely different tool than a coaxial wire stripper or twisted pair stripper. It is always worth reading the manufacturer's information and specifications.

Products: 3

Warehouse:

TME
All
Page 1
NEW
Stripping tool; 18AWG,20AWG,22AWG,24AWG,26AWG,28AWG,30AWG
Manufacturer part number: PAW-24
Manufacturer: ENGINEER
Net price for quantities from 1 pcs - 35.66 USDGross price for quantities from 1 pcs - 35.66 USD
Net price for quantities from 5 pcs - 28.52 USDGross price for quantities from 5 pcs - 28.52 USD
Net price for quantities from 10 pcs - 25.70 USDGross price for quantities from 10 pcs - 25.70 USD
20 in TME stock
No. of pieces (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
NEW
Accessories: crimping jaws
Manufacturer part number: 4320-0301
Manufacturer: PRESSMASTER
Net price for quantities from 1 set - 37.27 USDGross price for quantities from 1 set - 37.27 USD
Net price for quantities from 3 set - 34.71 USDGross price for quantities from 3 set - 34.71 USD
0 in TME stock
No. of complete sets (Multiplicity: 1)
Minimum order quantity: 1.
Multiplicity: 1.
NEW
Stripping tool
Manufacturer part number: 100746
Manufacturer: CIMCO
Net price for quantities from 1 pcs - 142.83 USDGross price for quantities from 1 pcs - 142.83 USD
Net price for quantities from 3 pcs - 133.91 USDGross price for quantities from 3 pcs - 133.91 USD
Net price for quantities from 5 pcs - 124.98 USDGross price for quantities from 5 pcs - 124.98 USD