+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Bit - definition

A bit is the basic unit of information in digital systems, corresponding to a single logical state that can assume one of two values: 0 or 1. The term is derived from binary digit. A bit is the fundamental building block of all digital operations and represents the smallest possible fragment of data used in computing, electronics, and telecommunications.

In the context of computer memory and data processing, a bit represents the simplest form of information encoding—for example, the presence or absence of a signal, a high or low voltage level, or the selection between two logical states. In microprocessor architecture, bits are grouped into larger units such as bytes or machine words, enabling more complex computational and logical operations.

Bits are used in both binary data representation and data transmission systems, where link bandwidth is measured in bits per second (bps). They also form the basis of cryptographic algorithms, data compression methods, digital logic circuits, and control structures in computer systems. In digital electronics, each bit can be physically realized using components such as transistors or capacitors, which store its logical state in static or dynamic memory cells.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO