+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Coulomb (C) - definition

Coulomb (C) is the SI base unit of electric charge, defined as the amount of charge transported by a current of one ampere in one second. It represents a measure of the quantity of electricity and describes the ability to exert electrostatic influence and participate in current conduction processes. In its modern definition, the coulomb is indirectly established through the elementary charge constant, whose value was fixed as an exact number during the 2019 redefinition of SI units.

The name “coulomb” derives from the French physicist Charles-Augustin de Coulomb, who conducted pioneering research on electrostatic forces. This unit plays a crucial role in describing electrical phenomena at both macroscopic and microscopic scales. In the context of elementary particles, one coulomb corresponds to the charge of approximately 6.24 × 10¹⁸ electrons or protons, each carrying an elementary charge of opposite sign.

In engineering practice, the coulomb is used to quantify charge flow in electrical circuits, determine the capacitance of capacitors, measure electrochemical effects, and analyze the movement of charged particles in electric fields. It is closely related to other units such as the ampere, volt, and joule, which together define the fundamental relationships in electrical engineering, including Ohm’s and Coulomb’s laws. Quantities expressed in coulombs are essential in calculations involving energy storage and transfer, particularly in battery technology, capacitors, and power conversion systems.

As a fundamental unit, the coulomb also enables the quantitative description of electrostatic and electromagnetic phenomena, such as electric field strength, electrostatic force, and charge density. Its applications span a wide range of disciplines, from theoretical physics to power engineering and consumer electronics.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO