+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Reactance - definition

Reactance is the imaginary component of complex impedance, describing the opposition to alternating current (AC) flow presented by passive elements in an electrical circuit that do not dissipate energy as heat. Unlike resistance, reactance does not consume energy but temporarily stores and releases it in electric or magnetic fields, resulting in a phase shift between voltage and current. The value of reactance depends on the signal frequency and the type and parameters of the circuit element.

Reactance occurs in two forms: inductive and capacitive. Inductive reactance is associated with coils and arises from the magnetic field resisting changes in current, whereas capacitive reactance appears in capacitors due to variable voltage generating alternating charge flow in the electric field. Inductive reactance increases with frequency, while capacitive reactance decreases, which is critical in designing filters, resonant circuits, and impedance matching networks.

In AC circuits, reactance affects the overall behavior of the circuit, including signal amplitudes and phase shifts. It is expressed in ohms but takes imaginary values - positive for inductance and negative for capacitance - allowing the use of complex number calculus in the analysis of intricate electrical networks. Along with resistance, reactance determines [impedance](/au/en/news/library-articles/page/61900/, the total electrical opposition influencing both active and reactive power flow in power systems.

Understanding and accurately calculating reactance is essential in fields such as power engineering, analog electronics, telecommunications, and high-frequency circuit design. Considering reactance enables circuit optimization, signal distortion reduction, minimized losses, and improved energy efficiency of devices.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO