+1 500 000 products in offer

7000 packages per day

+320 000 clients from 150 countries

Quick Buy Favourites
Cart

Digital signal - definition

Digital signal is a time-discrete signal that assumes a finite number of value levels, most commonly represented in binary form as sequences of zeros and ones. It serves as the fundamental carrier of information in digital systems, where data is processed, transmitted, and stored as sequences of logical symbols. In contrast to an analog signal, which varies continuously, a digital signal exhibits step-like changes in value at defined time intervals, which simplifies its analysis, processing, and resistance to interference.

A digital signal is typically represented using two voltage levels corresponding to logical states: low (0) and high (1). This format enables unambiguous interpretation of the signal even in the presence of noise or transmission path variations. As a result, digital signals are widely used in electronic devices, computer systems, automation, and telecommunications, forming the basis of microprocessors, computers, FPGA circuits, and digital network data transmission.

In digital systems, data is processed through logical, arithmetic, and sequential operations executed by digital circuits. A digital signal can be generated directly in digital form or derived from analog signals through an analog-to-digital converter (ADC). Conversely, when digital data must be transferred to analog systems, digital-to-analog converters (DACs) are used. The sampling rate and resolution of converters determine the accuracy with which the original analog signal is represented.

Digital signals enable the implementation of complex processing algorithms, compression techniques, and error correction mechanisms, allowing for efficient and reliable information transmission. Owing to the unambiguous nature of logical state representation, digital signals are much easier to replicate, store, and secure than analog signals, which accounts for their dominant role in modern technological systems.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO