+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

USB - definition

USB (Universal Serial Bus) is a universal serial interface developed to standardize communication between computers and peripheral devices. This standard enables both data transmission and electrical power delivery between a host (e.g., a computer) and connected devices such as keyboards, mice, printers, cameras, storage media, or smartphones. USB replaced earlier, less versatile interfaces by offering simplified installation, automatic hardware detection (plug and play), and hot-swap functionality, allowing devices to be connected and disconnected without shutting down the system.

The USB standard has undergone several evolutionary stages since its introduction in the 1990s. Successive versions (USB 1.1, 2.0, 3.0, 3.1, 3.2, and USB4) introduced significant improvements in data transfer speeds, power efficiency, and functionality. The latest versions offer bandwidths reaching tens of gigabits per second, supporting demanding multimedia applications and powering high-consumption devices, including laptops and monitors.

USB architecture is based on a star topology, where a central host communicates with multiple peripheral devices via hubs. The interface uses packet-based data transmission and features a flexible communication protocol tailored to different device classes. At the physical layer, various connector types are used, with USB-A, USB-B, and USB-C being the most common—the latter enabling reversible connection and integrating data, video, and power functions into a single interface.

USB is not limited to wired communication; it also includes USB OTG (On-The-Go) technology, which allows devices to act as either host or client without a computer. Thanks to its versatility and ongoing technological advancement, USB has become one of the most widespread communication interfaces in consumer, industrial, and professional electronics.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO