+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
Particle accelerator is a device used to impart very high kinetic energies to charged elementary particles, such as electrons, protons, or ions, by accelerating them using electric fields and directing their motion using magnetic fields. Such machines are used in fundamental research in particle physics, nuclear physics, materials engineering, medicine, and industrial technology.
The principle of operation of an accelerator is based on accelerating particles to speeds close to the speed of light in a specially designed track. Depending on the design, acceleration can occur in a straight line (linear accelerators) or in a closed ring (cyclic accelerators, such as cyclotrons and synchrotrons). Individual acceleration pulses are synchronized with the movement of the particles to gradually increase their energy while maintaining control over their trajectory.
Accelerators enable the study of the structure of matter at the deepest level, allowing for collisions between particles with tremendous energy, resulting in the creation of new elementary particles, recorded using precise detectors. Analyzing these processes provides information about fundamental physical interactions and the properties of matter under extreme conditions.
Beyond high-energy physics, accelerators are also used in cancer therapies (e.g., proton radiation therapy), production of radioisotopes, medical sterilization, as well as in semiconductor technology and non-destructive material research. In medicine and industry, smaller accelerators with limited power and size are often used, designed for specific practical tasks.
The development of accelerators is one of the pillars of modern experimental physics, and their operation requires strict control of beam parameters, high vacuum, advanced electronics, and complex monitoring systems. In the largest installations of this type, such as the Large Hadron Collider (LHC), energies are achieved that allow for the exploration of phenomena that occurred directly after the Big Bang.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.