+1 500 000 products in offer
7000 packages per day
+320 000 clients from 150 countries
A galvanic cell, also called electrochemical cell, is a device that converts chemical energy into electrical energy as a result of redox reactions occurring at the interface between two electrodes immersed in electrolyte. Its operation is based on the separation of oxidation and reduction half-reactions, which leads to a potential difference between the electrodes and allows the flow of an electrical charge in an external electrical circuit.
The basic structure of the cell consists of the anode, where the oxidation process takes place, and the cathode, where the reduction takes place. Electrodes are made of conductive materials, often metals, alloys or compounds with catalytic properties. The conductive medium inside the cell is the electrolyte, which allows the transport of ions between the electrodes, ensuring that the ionic circuit is closed and the electrochemical equilibrium is maintained.
The characteristics of a galvanic cell depend on the type of electrode materials used and the chemical composition of the electrolyte, which affects the standard voltage and energy conversion efficiency. In galvanic cells, such as Daniella cells or lithium-ion cells, the process of spontaneous electron flow generates an electrical voltage, which can be used as a power source. In galvanic cells, where an external voltage is applied, the reverse processes occur, leading to energy storage in chemical form, which is the basis of Rechargeable Batteries and electrolysis systems.
The efficiency of a cell depends on parameters such as current density, internal impedance and the thermodynamic stability of the electrochemical system. High-energy cells used in energy storage technology use advanced electrode materials such as transition metal oxides, nanostructured carbon conductive carriers and ceramic composites, which improve the kinetics of electrochemical reactions and increase the energy capacity of the system.
In modern applications, galvanic cells are the cornerstone of battery and rechargeable battery technologies used in consumer electronics, electric motoring and renewable energy systems. Fuel cell technologies use the electrochemical oxidation phenomena of gaseous or liquid fuels, such as hydrogen or methanol, to generate electricity in an efficient and environmentally friendly manner.
Advanced electrolytic cell energy management systems use redox process modelling methods, predictive load management algorithms and temperature control and voltage stabilisation systems to optimise cell operation under dynamic load conditions and minimise active material degradation. High-performance solid electrolyte technologies and hybrid electrochemical designs are enabling further development of cells with increased energy density, longer life and greater resistance to extreme environmental conditions.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.