+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Pentode - definition

The Pentode is a vacuum electron tube belonging to the multigrid tube group, containing five electrodes: the cathode, the anode, and three grids - control, shielding and attenuation. It was developed in the 1920s as a development of the triode and tetrode, with the aim of improving the amplification performance of electrical signals, especially in terms of linearity and stability of operation at higher frequencies.

The primary function of the pentode is to amplify a voltage or current signal in analogue circuits. The control grid, located closest to the cathode, controls the flow of electrons emitted by the glowing cathode. The shielding grid reduces the inter-electrode capacitance between the anode and the control grid, which reduces feedback and improves the stability of the amplifier. The damping grid, placed between the shielding grid and the anode, eliminates secondary electron emission from the anode that could interfere with tube operation, especially at high anode voltages.

Thanks to the use of three grids, pentodes offer much higher voltage gain than triodes and better dynamic characteristics in low- and high-power amplifier circuits. They are distinguished by their high input impedance, low input and output capacitance, and ability to operate at high voltages and frequencies. In practical applications, pentodes have been used in RF circuits, audio amplifiers, oscillators and detectors, both in consumer and professional technology.

Over time, with the development of semiconductor technology, pentodes have largely been replaced by transistors, but they are still used in some areas, especially in audiophile tube amplifiers and specialised equipment, due to their characteristic sonic properties and linear operating characteristics.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO