+1 500 000 products in offer

6000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Grid computing - definition

Grid computing is a model of distributed computing, involving the sharing of computing resources from multiple, often geographically dispersed, independent computer units. Unlike traditional centralised systems, grid computing creates a dynamically juxtaposed computing environment in which individual computers work together as elements of a single virtual supercomputer.

Resources in grid computing include not only computing power, but also Mass Storage, software and specialised devices that are made available through standard communication protocols and middleware platforms. A key aspect of grid computing is the ability to automatically allocate tasks to the nodes available at any given time, thus optimising the use of available resources and balancing the load on the system.

Grid systems are characterised by high scalability, flexibility and resilience to single component failures. However, they require a sophisticated management mechanism that addresses authorisation, security, data synchronisation and task scheduling. Due to its structure, grid computing is used in computationally intensive areas such as numerical modelling, data analysis scientific, simulation engineering or big data mining.

Grid solutions are the foundation of many research and commercial projects, including large-scale computing initiatives and shared IT infrastructure. With the development of cloud technologies and containerisation, the concept of grid computing has taken on new importance as part of broader distributed computing architectures.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO