+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

IP degree of protection - definition

IP (ingress protection) rating is a standardised classification that defines the level of protection of an electrical or electronic equipment enclosure against the penetration of solids, dust and liquids, including water. The IP marking system is defined by IEC 60529 and consists of the letters 'IP' and two digits. The first characterises resistance to the penetration of physical objects and dust, while the second refers to resistance to the effects of moisture, water or liquids under specific exposure conditions.

The use of the IP designation is indispensable in the context of the design, manufacture and operation of equipment used in exposed environments, such as industrial installations, Building Automation, lighting systems, laboratory equipment or Measuring Instruments. Adequate sealing protects active components from mechanical damage, short circuits, corrosion and failures due to moisture or dust, which translates into an extended device life cycle and increased user safety.

Interpretation of the IP code requires knowledge of assigned numerical values that define specific test conditions, such as water pressure, exposure time, particle size or immersion depth.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO