+1 500 000 products in offer
6000 packages per day
+300 000 clients from 150 countries
Static electricity is a physical phenomenon associated with the accumulation of an electrical charge on the surface of a body that is not in a state of conduction. It arises from the separation of electrical charges, usually due to friction, contact or electrostatic induction between different materials. Unlike electric current, which involves the flow of electrons, static electricity refers to a state in which charges remain at rest, often accumulating locally and maintaining an electrical potential relative to their surroundings for a period of time.
The process of static electricity involves the transfer of electrons from one body to another, leading to an excess of negative charge in one place and a deficiency in another. Such charged bodies interact with each other according to Coulomb's law and the accumulated charge can lead to phenomena such as sparks, corona discharges or the attraction of small particles. In many cases electrostatic discharge occurs rapidly, accompanied by the emission of light, sound and heat.
Static electricity is commonly observed in everyday life, e.g. when removing plastic Clothing, combing dry hair or walking across a carpet in a dry room. In industry and technology, it can lead to interference with electronic equipment, damage to semiconductor components and fire hazards in combustible environments. For this reason, protective measures such as earthing, air Ionizers, anti-static bands or suitable electroconductive materials are used.
Static electricity phenomena are also important in electrostatic painting, material separation, printing and air filtration. In the natural sciences and engineering, static electricity is the starting point for analysing more complex electrostatic interactions and the properties of dielectric materials.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.