+1 500 000 products in offer
6000 packages per day
+300 000 clients from 150 countries
FORTRAN (Formula Translation) is one of the oldest high-level programming languages, designed in the 1950s by an IBM team led by John Backus. Its main purpose was to allow mathematical and scientific calculations to be written efficiently in a form that approximated algebraic notation, greatly simplifying the development of programs compared to low-level machine code. FORTRAN was the first language to allow automatic compilation of source code into executable form, revolutionising the approach to computer programming.
The FORTRAN language is distinguished by its simple, concise syntax and high performance, making it particularly suitable for engineering, numerical and scientific applications. In particular, it has found widespread use in areas such as computational mechanics, structural analysis, physical simulations, fluid dynamics and quantum computing, where operations on matrices, vectors and floating point numbers dominate.
FORTRAN has undergone a number of standards evolutions, from FORTRAN I and FORTRAN IV, through FORTRAN 77, to the more modern FORTRAN 90, 95, 2003, 2008 and 2018, with each successive version introducing language extensions such as dynamic memory management, modular programming, support for abstract types, parallelism and compatibility with object-oriented standards. Despite the emergence of new programming languages, FORTRAN remains an essential tool in scientific and computing environments where maximum performance and a proven infrastructure are important.
One of the key advantages of FORTRAN is the advanced code optimisation by Compilers, which can generate very fast executable code, especially for applications that make intensive use of arithmetic operations. As a result, the language still forms the basis of many numerical libraries, simulation packages and large engineering systems whose maintenance and development require precision, stability and high computational efficiency.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.