+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Heterodyne - definition

Heterodyne is a frequency-dependent auxiliary signal used in radio and electronic technology to realise a frequency conversion, known as mixing. The term also refers to the process of heterodyne itself, a non-linear combination of two signals that results in new frequency components that are the sum and difference of the frequencies of the input signals. Heterodyne is most often generated by a local oscillator, and its use enables the radio signal to be shifted from one part of the spectrum to another - usually to a so-called intermediate frequency (IF), more convenient for further processing.

The concept of heterodyning underpins the operation of a superheterodyne radio receiver - a system in which the input signal is mixed with a heterodyne signal to produce a stable, fixed intermediate frequency independent of the frequency of the received channel. This approach simplifies the design of filters and amplifiers, enables precise tuning and improves the selectivity and sensitivity of the system.

Heterodyning is also used in radar technology, satellite communication systems, Spectrum Analyzers, musical instruments and acoustic signal processing. The process relies on the properties of non-linear electronic components such as Diodes, Transistors or Integrated circuits to produce new spectral components.

From a physical point of view, heterodyne results from the multiplication of two sinusoidal waveforms in the time domain, resulting in components with frequencies that are the sum and difference of the original signals. Choosing one of these - usually the one with the lower frequency - allows further analysis and processing of the signal to be simplified without losing the information it contains.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO