+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
Parallel port is a communication interface that allows the simultaneous transmission of multiple bits of data over multiple signal lines. Unlike the serial port, which transmits data bit by bit over a single line, the parallel port uses several wires, each responsible for one bit, allowing faster transmission of information over short distances. It was commonly used in personal computers to connect peripherals, especially printers, scanners, memory programmers and industrial equipment.
The standard type of parallel port on PCs was the Centronics interface, later developed into the IEEE 1284 standard, which allowed not only unidirectional data transfer but also bi-directional communication and support for modes such as nibble, byte, ECP (Extended Capabilities Port) and EPP (Enhanced Parallel Port). The physical connector was usually in the form of a 25-pin D-sub connector (DB-25), and signal lines included control and status signals such as 'strobe', 'acknowledge' and 'busy' in addition to data.
Parallel ports were also widely used in microcontrollers as general-purpose ports I/O, allowing multiple data lines and control signals to be handled in parallel. By directly accessing the individual bits of the port, it was possible to precisely control external digital and analogue devices, as well as to implement custom communication protocols at the hardware level.
Despite their historical importance and high versatility, parallel ports have largely been superseded by faster and more versatile serial interfaces such as USB, SPI or I²C, which offer fewer wires, higher transmission reliability and better integration into integrated circuits. Nevertheless, in some specialised, industrial and educational applications parallel ports are still used because of the simplicity of implementation and ease of diagnostics.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.