+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Fahrenheit Scales - definition

The Fahrenheit Scales is a thermometric temperature scale developed in the 18th century by the German physicist Daniel Gabriel Fahrenheit. It was defined based on observations of the characteristic points of chemical mixtures and states of matter of water, but its modern version is related to precise measurements of the properties of water at standard atmospheric pressure. On this Scales, the freezing point of water is 32°F and the boiling point is 212°F, giving an interval of 180 degrees between these points.

The unit of temperature on this scale is the degree Fahrenheit, denoted by the symbol '°F'. This degree is smaller than the degree Celsius, and converting values between these scales requires a formula that takes into account both the aspect ratio and the offset of the zero reference point. The Fahrenheit scale is considered to be non-linear to the absolute scale, but in practice gives sufficient accuracy for technical and environmental applications.

The system is currently used mainly in the United States and in several other countries, where it functions as a standard in meteorology, construction and the industry HVAC. Despite the global dominance of the Celsius scale and the Kelvin scale in science and engineering, the Fahrenheit Scales remain culturally and functionally relevant in regions that have maintained its use. Its design, based on a more extended range of use in everyday weather conditions, means that it offers greater resolution in describing changes in ambient temperature.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO