+1 500 000 products in offer

6000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Joule (J) - definition

The joule (J) is the SI unit of energy, work, and heat, defined as the amount of energy transferred or used when a force of one newton (N) moves an object one meter in the direction of the force. The unit is named after the English physicist James Prescott Joule, who conducted pioneering research on the interconversion of mechanical and thermal energy.

In physics and engineering, the joule applies to various forms of energy, including kinetic, potential, thermal, electrical, and electromagnetic energy. It may represent the work done by a motor, the energy consumed by an electrical device, the heat released by a substance, or the energy stored in a capacitor. The joule is a derived unit and can also be expressed as a newton-meter (N·m), reflecting its relationship with the base units of mass, length, and time.

The joule is widely used in engineering calculations, energy system design, thermodynamic analysis, and efficiency measurements of devices and processes. In the context of electrical energy, one joule corresponds to the work done when a current of one ampere (A) flows through a resistance of one ohm (Ω) for one second. In practical applications, particularly in power engineering and electronics, multiples such as kilojoule (kJ) and megajoule (MJ) are commonly used to describe larger quantities of energy.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO