+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
Photon is an elementary physical particle that acts as the quantum carrier of electromagnetic interactions and transports a discrete amount of light energy. In quantum mechanics, a photon is described as a massless boson with spin 1, propagating at the speed of light in a vacuum. Its energy is directly proportional to the frequency of the associated electromagnetic wave.
In the wave-particle duality model, the photon exhibits both particle-like and wave-like properties, meaning it can be described as both a quantized packet of energy and a wave propagating through space. This dual nature explains phenomena such as interference, diffraction, photoemission, and Compton scattering. A photon carries no electric charge or magnetic moment, and thus does not interact directly with electric or magnetic fields, but it can interact with charged particles, excite atoms, or trigger photoelectric effects.
In physics and engineering, the photon plays a fundamental role in the description and application of light and other forms of electromagnetic radiation. It is the primary agent in the emission and absorption of radiation in atomic and molecular systems, as well as a carrier of information in optoelectronic, telecommunication, and quantum technologies. In astrophysics, photons enable the observation of cosmic phenomena across different spectral ranges, while in biology and medicine they are used in diagnostics and light-based therapies. The properties of photons are also harnessed in advanced laser systems, photosensitive sensors, and quantum cryptography.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.