+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

LiDAR (Light Detection and Ranging) - definition

LiDAR (Light Detection and Ranging) is a remote sensing technology for distance measurement and spatial modeling based on the analysis of reflected laser light pulses. It operates by emitting short laser beams toward a target surface and measuring the time it takes for the pulses to return after bouncing off objects. Based on this time interval, the system calculates precise distances, generating a highly accurate three-dimensional representation of the environment.

A typical LiDAR system consists of a laser pulse emitter, a detection receiver, and synchronization and data processing units. Unlike radar technologies that use radio waves, LiDAR employs light—typically in the near-infrared spectrum—allowing for higher spatial resolution. LiDAR devices can be mounted on aerial platforms, ground vehicles, drones, or used in stationary geodetic surveys.

LiDAR technology is applied across various fields, including cartography, geoinformatics, civil engineering, archaeology, forestry, autonomous systems, safety, and the automotive industry. In automotive applications, it is a key solution for real-time environment mapping, supporting advanced driver-assistance systems (ADAS) and autonomous vehicles. In geodesy, it enables the creation of precise digital terrain and surface models, even in hard-to-reach or forested areas.

The high measurement resolution and capability to operate under diverse environmental conditions make LiDAR a crucial tool in spatial analysis and automation of environment perception processes. Data generated by LiDAR systems is often processed using advanced algorithms, such as object recognition, segmentation, or point cloud generation, enabling integration with geographic information systems (GIS), 3D modeling, and AI-based solutions.

LIDAR sensor modules

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO