+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
Acoustics is the branch of physics that deals with the study of sound waves, their formation, propagation, interaction with matter and reception by the sense organs. The subject of acoustics is all phenomena connected with vibrations of particles in elastic media, such as air, water or solids, which lead to the propagation of mechanical waves in the audible frequency range, infrasound i ultrasonic.
The field of acoustics covers both theoretical, as well as practical ones. The theoretical research examines the laws governing wave propagation, their interference, diffraction and attenuation. Applied acoustics focuses on solving problems related to noise control, improvement of sound quality in architectural spaces, design of sound reinforcement systems, as well as the use of ultrasound in medicine, industry and non-destructive testing.
The structure of this field includes numerous sub-fields, such as psychoacoustics, which is concerned with human perception of sound, electroacoustics, which deals with the processing of acoustic signals by means of electronic devices, or bioacoustics, which analyses sound communication in the animal world. Environmental acoustics also plays an important role, which aims at assessing and reducing acoustic nuisance in the human environment.
The development of digital technology has made it possible to significantly improve methods of sound measurement and analysis, which finds application in sound engineering, speech synthesis, voice recognition and active noise reduction systems. Acoustics remains an interdisciplinary field, combining physics, engineering, computer science, biology and psychology to better understand and exploit sound phenomena.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.