+1 500 000 products in offer
7000 packages per day
+320 000 clients from 150 countries
Response time is a quantity describing the delay between the moment a stimulus (input, signal, change in conditions) occurs and the response of a system or technical device. Others use the concept in a variety of fields - from Automation and electronics to computer science, optics and ergonomics. From a technical point of view, the response time informs about the efficiency of the system, its ability to track changes and the speed of the response relative to the desired control signal.
In control and control systems, the response time determines the rate at which the system reaches a state of equilibrium after a disturbance or change in the setpoint. The shorter this time, the faster the system adjusts its performance, which is important for dynamic and precise processes. In electronics, for example in sensors or optoelectronic components, response time refers to the time it takes for a signal to be recorded and transmitted for further processing.
In liquid crystal displays (LCD) or light-emitting diode (OLED) displays, the response time determines how quickly a pixel can change its state between different brightness levels. This parameter affects the sharpness of the image when displaying dynamic content, minimising the effect of ghosting. In the context of computer systems, response time can also refer to the response time of an operating system or application to a user request.
In security and Automation systems, it is important that the response time is within the limits set by standards, as exceeding it can lead to erroneous actions or dangerous situations. In high-precision and high-reliability applications, response time is one of the basic parameters for assessing system quality.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.