+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
Potential energy is the form of mechanical energy associated with the position of an object in a field of conservative forces, such as a gravitational, electrostatic or elastic field. It represents the ability of a system to perform work as a result of changes in the spatial configuration of bodies under the influence of internal or external interactions. This energy does not manifest itself directly as motion, but is stored in the system and can be transformed into kinetic energy or other forms of energy as physical processes occur.
For a gravitational field, potential energy depends on the mass of the body, the acceleration of the earth and its height relative to an assumed reference level. For an electrostatic field, it is described by the position of the charge relative to other charges or sources electric potential. In elastic systems, such as springs or beams, the potential energy is a function of the deformation and the elastic coefficient of the material, according to Hooke's law.
A characteristic feature of potential energy is its dependence on the configuration of the system rather than its actual velocity. A change in this energy when moving a body in a field of conservative forces leads to an equivalent gain or loss of kinetic energy, according to the principle of conservation of mechanical energy. In the dynamic analysis of physical systems, potential energy is used to define the Lagrange and Hamiltonian functions, which allows movement to be described in a general way and independent of any particular reference system.
In electrical engineering, the concept is used in the analysis of the energy stored in the electric fields of Capacitors and in circuit theory, where potential energy corresponds to the voltage stored in energy storage elements. On the atomic and molecular scales, it describes interactions between particles and influences the stability of chemical structures and the course of physicochemical reactions.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.