+1 500 000 products in offer

7000 packages per day

+320 000 clients from 150 countries

Quick Buy Favourites
Cart

Beater (knypel) - definition

A beater, also known as a knuckle, is a hand tool used in assembly, workshop and construction operations whose main function is to transmit a controlled percussive force to a workpiece or other tool, such as chisel, chisel or drift. The design of a beater usually includes a solid body in the form of a cylinder or block with rounded edges, made of a deformation-resistant material, often hardwood, plastic, technical rubber, brass or steel, depending on the purpose and type of work.

Beaters are used wherever precise control of impact force is required while minimising the risk of damage to the surface of the workpieces. In precision assembly techniques, especially when working with parts that are prone to distortion, beaters made from soft plastics or wood allow force to be applied without the risk of scratching or deforming the material. Heavy engineering applications, on the other hand, use steel or brass beaters that can carry significant dynamic loads while maintaining shape stability.

In metalworking, carpentry, stonemasonry and renovation operations, the beater acts as an auxiliary tool to properly align, fit or separate components. The ergonomic shape and appropriate weight of the beater help to reduce operator fatigue and increase precision. Specialised industrial applications also use anti-spark beaters made of non-magnetic and non-sparking materials for use in explosive environments.

Hammers and Axes

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO