+15,00,000 products in offer
7,000 packages per day
+3,00,000 clients from 150 countries
The capacitor capacity calculator facilitates the calculation of the equivalent capacitance of series and parallel circuits – whether you are working with individual components or several capacitors connected together. Just enter the capacitor values, select the appropriate units (picofarad – pF, nanofarad – nF, microfarad – µF, millifarad – mF, farad – F), and the tool will automatically convert them to a common base and provide the result. This is a practical aid when selecting replacements, designing filters, power supplies, or timing circuits.
The capacitor calculator helps quickly calculate the equivalent capacitance of several elements connected in series or parallel, without manual calculations and juggling units. It is useful wherever a capacitance value not directly available in the catalogue is needed or when several capacitors must be selected as a substitute for one element with an unusual rating. This makes it easier to select capacitors for an existing design, optimize a filter, match an RC timing circuit, or estimate the real capacitance in a repaired power supply.
The basic capacitance unit in the SI system is the farad (F), but in practice, it is usually encountered in the form of derived units. Typical capacitors in electronics have capacitances ranging from single picofarads to hundreds of microfarads, so it is more convenient to work with smaller units. The capacitor capacitance calculator automatically converts between:
In high-frequency (RF) circuits, capacitors in the pF and nF range dominate; in filters and coupling circuits, nF is often used; and in power supplies and ripple filtering, usually µF. The calculator allows freely combining different units in one calculation, which facilitates working with mixed capacitance values.
In a series connection of capacitors, the equivalent capacitance is smaller than the smallest capacitance in the given arrangement. This results from the fact that capacitors in series "share" the voltage, and the charge flowing through each element is the same. Mathematically, the sum of the reciprocals of the individual capacitor capacitances gives the reciprocal of the total equivalent capacitance of the entire network.
Such a connection is used, among others, when it is necessary to increase the allowable operating voltage – for example, when working with higher supply voltages and the available capacitors have too low nominal voltage. The calculator quickly checks what the total capacitance of such a series will be and how much it differs from the single, "target" value.
In a parallel connection of capacitors, capacitances simply add up, and the voltage across each element is the same. This makes it easy to increase the total capacitance of the network by adding more capacitors in parallel to an existing element. This is especially helpful when needing to "top up" to an unusual capacitance value or improve ripple filtering in a power supply.
Parallel connections are commonly used in power filters, where capacitors of different capacitances (e.g., 100nF + 10µF) are combined to more effectively suppress both fast disturbances and slower voltage changes. The capacitor capacitance calculator quickly calculates the total capacitance of such a set regardless of whether the individual elements are given in pF, nF, or µF.
In practical servicing, the capacitor calculator facilitates selecting substitutes – for example, when you want to replace a hard-to-get 47nF capacitor with two 100nF capacitors connected appropriately. When designing PCB boards and power supplies, the tool allows quickly checking whether a set of available capacitors will provide sufficient filtering capacitance and whether the values fit within the required range. In analog, audio, and RC filter circuits, the calculator speeds up selecting capacitances for given time constants and facilitates experiments with different configurations.
However, when working with capacitors, it is always worth remembering that proper operation of the circuit depends not only on capacitance but also on operating voltage, ESR, tolerance, and dielectric type.
Yes. From the point of view of capacitance calculations, bipolar and polarized capacitor circuits are calculated exactly the same – the formulas for series and parallel connections are identical regardless of dielectric type or polarity. Therefore, the calculator shows the correct equivalent capacitance but does not check for you whether a given capacitor type may be used at a specific location – electrolytics still require observing polarity, operating voltage, and signal type (DC/AC).
Yes, different types of capacitors can be combined, and in many circuits, this is even a standard solution – e.g., a large-value electrolytic capacitor in parallel with a 100nF ceramic at the power supply. However, you must remember several rules: all elements must have appropriate operating voltage, electrolytic capacitors must be polarized according to marking, and in precision circuits, differences in ESR, leakage current, and temperature stability must be considered. Mixing types "blindly" can be problematic in audio filters, measurement circuits, or high-frequency circuits – where a more conscious approach is advisable.
In a series connection, each capacitor "receives" a part of the total voltage, so its nominal voltage cannot be lower than the voltage that may appear across it. If the capacitors are identical, it is generally assumed that the voltage divides equally – then the maximum operating voltage of the circuit is approximately the sum of the nominal voltages, but it is still worth leaving a margin. In practice, due to differences in capacitances and leakage currents, the voltage does not divide perfectly equally; therefore, in circuits with higher voltages, capacitors with greater margins are usually used, and – for more demanding applications – balancing resistors are employed.
In parallel connection, all capacitors see the same voltage, and their charges add up. Therefore, capacitances simply add, and the equivalent capacitance is greater than any single one. In series connection, the situation is the opposite: capacitors are "connected one after another", the charge flows through them at the same current, and the effective distance between plates increases. Therefore, the equivalent capacitance is smaller than the smallest capacitance. Mathematically, in series, reciprocals (1/C) sum up, and in parallel, the capacitances themselves (C) sum.
It depends on what is more important in the given circuit: simplicity, PCB space, electrical parameters, or component availability.
A single larger capacitor works better when:
Several smaller capacitors connected in parallel are better when:
In practice, a combination of both approaches is often used: one larger "energy storage" capacitor and several smaller ones placed closer to integrated circuits. In case of doubts – especially with higher power and high frequencies – it is worth consulting manufacturer application notes or consulting the design with an experienced PCB designer.