+15,00,000 products in offer

7,000 packages per day

+3,00,000 clients from 150 countries

Quick Buy Favourites
Cart

Logic gate - definition

A logic gate is a fundamental functional element of digital circuits that performs logical operations on one or more binary input signals. Physically, it operates as an electronic circuit that receives input signals in the form of two logic levels—typically represented as 0 and 1—and produces a single output signal based on a specific logical rule. Each gate implements a Boolean function, such as conjunction (AND), disjunction (OR), or negation (NOT), as defined by Boolean algebra.

Logic gates form the basis for constructing more complex digital systems, including counters, registers, flip-flops, and ultimately microprocessors and embedded computer systems. By combining multiple gates in structured configurations, it is possible to process signals, perform calculations, make logical decisions, and control the operation of electronic devices. Logic gates can be physically implemented using various technologies, such as bipolar transistors, MOSFETs, or programmable integrated circuits.

The operation of logic gates is deterministic and occurs in real time, which enables the development of fast and reliable systems in automation, telecommunications, and computer engineering. Due to their universality and modular nature, logic gates are the foundation of modern digital design, whether in integrated systems or in solutions based on programmable logic.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO