+13,00,000 products in offer

7,000 packages per day

+3,00,000 clients from 150 countries

Quick Buy Favourites
Cart

FM (frequency modulation) - definition

FM (frequency modulation) is an analog modulation technique in which the frequency of a carrier wave is varied in accordance with the instantaneous amplitude of the input information signal, while its amplitude remains constant. Unlike amplitude modulation, where information is conveyed through changes in signal level, FM encodes information by varying the spacing between successive peaks of the carrier wave.

The principle of FM operation is that the higher the amplitude of the modulating signal, the greater the deviation of the carrier frequency from its nominal value. In this way, the information signal causes the cycles of the carrier wave to stretch or compress, resulting in a modulated signal with a characteristic spectrum whose bandwidth depends on the modulation amplitude and frequency. The receiver demodulates the signal by analyzing these instantaneous frequency variations to recover the original information.

FM is widely used in radio communications, particularly for broadcasting audio signals in the VHF band, where it provides high sound quality and strong immunity to interference. Since electromagnetic noise affects amplitude more than frequency, FM offers superior reception quality compared to other analog modulation methods. In digital technology, its equivalent includes frequency-based modulation schemes with discrete levels, such as FSK (Frequency Shift Keying), used in modems and data transmission systems.

In electronic and telecommunication systems, FM is also employed in radar, telemetry systems, and wireless control circuits. Selecting appropriate frequency modulation parameters enables efficient use of available bandwidth, improves transmission quality, and increases the reliability of data transfer in the presence of noise or interference.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO