+15,00,000 products in offer

7,000 packages per day

+3,00,000 clients from 150 countries

Quick Buy Favourites
Cart

Electromagnetic compatibility (EMC) - definition

Electromagnetic compatibility (EMC) is the ability of an electronic device or system to operate correctly within its electromagnetic environment without causing interference that could adversely affect the performance of other devices. This means both limiting the electromagnetic disturbances emitted by the device itself and ensuring its immunity to external electromagnetic interference. The concept of EMC covers the full range of interactions, including radiated and conducted emissions, as well as susceptibility to external radiation sources.

In engineering practice, EMC is essential for ensuring the reliability and safety of electronic systems, especially in environments with high equipment density such as industry, transportation, healthcare, telecommunications, and building automation. Failure to meet EMC requirements can lead to data transmission errors, control malfunctions, signal loss, or even equipment damage. Control systems, measuring instruments, and devices operating near strong sources of electromagnetic radiation are particularly sensitive to these issues.

EMC is based on two fundamental pillars: limiting the emissions generated by a device (emissivity) and ensuring sufficient immunity to external disturbances (electromagnetic immunity). Achieving EMC requires appropriate circuit design, shielding, signal filtering, grounding, and compliance testing against applicable international standards, such as those issued by IEC, CISPR, and EN. During the certification process of electronic devices, specialized EMC testing is performed to verify compliance with permissible emission levels and required immunity thresholds.

Electromagnetic compatibility is an interdisciplinary field encompassing electronics, wave physics, materials science, and measurement technology. Ensuring EMC is a prerequisite for the market approval of many products—especially in the European Union, where it is governed by the EMC Directive and related regulatory frameworks.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO