+15,00,000 products in offer

7,000 packages per day

+3,00,000 clients from 150 countries

Quick Buy Favourites
Cart

Microprocessor - definition

Microprocessor is an integrated electronic circuit that functions as the central processing unit (CPU) of a computer system, responsible for performing arithmetic, logic, control, and data processing operations based on stored instructions. It operates through a sequence of machine cycles, fetching instructions from memory, decoding them, and executing them in accordance with the instruction set architecture. The microprocessor is a fundamental component in digital systems, enabling computational, control, and communication tasks.

The core components of a microprocessor include an arithmetic logic unit (ALU), registers, an instruction decoder, a control unit, and data, address, and control buses. Modern microprocessors also incorporate auxiliary units such as cache memory, branch prediction mechanisms, memory controllers, and floating-point units, significantly enhancing performance. Multicore processors integrate several processing cores within a single chip, enabling parallel execution of multiple program threads.

Microprocessors are designed in various architectures, such as x86, ARM, MIPS, or RISC-V, each defining data organization, instruction types, and design philosophy. They are used in general-purpose computing devices like laptops, servers, and workstations, as well as in embedded systems, where they act as the central component of more complex control structures. Unlike microcontrollers, microprocessors do not include built-in RAM, program memory, or input/output peripherals, requiring external components and allowing for highly flexible and scalable system designs.

Advancements in microprocessor technology have led to significant increases in computational power, while simultaneously reducing size and energy consumption. As a result, microprocessors play a critical role not only in computer science but also in automation, telecommunications, industry, automotive systems, and in scientific and military applications. Their design and manufacturing rely on advanced lithographic techniques and electronic system engineering at the nanometer scale.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO