+15,00,000 products in offer
7,000 packages per day
+3,00,000 clients from 150 countries
Electric circuit is a closed system of interconnected conductive elements through which electric current can flow under the influence of an applied voltage. Its function is to transmit electrical energy and enable the controlled movement of electric charges between a power source and loads, in accordance with defined physical principles. The fundamental laws governing circuit behavior are Ohm’s law and Kirchhoff’s laws, which describe the relationships between voltage, current, and resistance, as well as the balance of currents and voltages at nodes and loops in the circuit.
An electric circuit structure may include voltage or current sources, passive components such as resistors, capacitors, and inductors, as well as active components like diodes, transistors, or integrated circuits. Current flows in a circuit only when the conductive path forms a closed loop, allowing electric charges to circulate under the influence of electromotive forces. Otherwise, if the circuit is open, the current flow is interrupted.
Circuits can be classified as direct current (DC) when the voltage and current remain constant over time, or alternating current (AC) when these quantities vary periodically. In more complex systems, dynamic and reactive dependencies are also considered, influencing the circuit’s time-domain and frequency-domain characteristics. Circuit analysis involves both static and dynamic aspects, including system response to input signals, stability, and energy efficiency.
Electric circuits form the foundation of all electronic devices and automation systems. Their design, modeling, and diagnostics require knowledge of electrical engineering principles, material properties, and interactions between components. Proper circuit function depends not only on correct connections but also on the physical parameters and quality of the components. In modern engineering, circuits are also analyzed for electromagnetic interference, energy efficiency, and compliance with technical standards.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.