+15,00,000 products in offer
7,000 packages per day
+3,00,000 clients from 150 countries
Radiometry is a branch of physics concerned with the measurement of electromagnetic radiation across the entire wavelength spectrum, regardless of its interaction with the human visual system. Its primary objective is to quantify the amount of radiant energy reaching a given point in space or emitted by a source. Radiometry provides tools for describing phenomena related to the emission, transmission, reflection, and absorption of radiation, and enables the analysis of the energetic characteristics of electromagnetic waves based on SI units.
Unlike photometry, which accounts for the subjective sensitivity of the human eye to visible light, radiometry treats all wavelengths equally, analyzing both visible and invisible radiation—such as infrared, ultraviolet, radio, or X-rays. Key physical quantities include irradiance, radiant luminance, radiant intensity, spectral distribution, and radiant flux density. Each of these parameters serves to precisely describe the amount of energy transferred per unit of time, area, solid angle, or wavelength.
Radiation measurements are carried out using devices known as radiometers, which can be calibrated for specific spectral bands and radiation types. Depending on the application, different detection methods are employed, such as absorptive, thermal, photonic, or bolometric techniques. Radiometry is applied in meteorology, astronomy, optical engineering, telecommunications, environmental monitoring, diagnostic medicine, and materials analysis. It is especially important in the design of optoelectronic systems, photovoltaics, thermal imaging, and the monitoring of natural and artificial electromagnetic radiation.
From a metrological perspective, radiometry requires precise detector calibration, elimination of environmental interference, and consideration of the geometric parameters of the measurement setup. This ensures accurate and repeatable results necessary for scientific analysis and technological quality control.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.