+15,00,000 products in offer
7,000 packages per day
+3,00,000 clients from 150 countries
Volt (V) is the SI unit of electric voltage, potential difference, and electromotive force. One volt is defined as the potential difference between two points of a conductor when a current of one ampere dissipates one watt of power. In general terms, the volt represents the ability of an electric field to perform work on a charge - the higher the voltage, the greater the energy per unit charge.
The concept of voltage is fundamental in power engineering, electronics, and field physics. Practically speaking, electric voltage represents the “driving force” enabling current flow in circuits. It can be generated by electrochemical sources (e.g., cells), electromagnetic sources (generators, transformers), or piezoelectric elements. The volt is a derived unit, expressed in terms of basic SI units as joule per coulomb (J/C), linking voltage to the work done by the electric field on a unit charge.
The volt is named after Italian physicist Alessandro Volta, the inventor of the first electrochemical cell. In technical applications, voltage is a key parameter in designing power supplies, transmission systems, and signal paths. Typical voltage values vary depending on the application—from millivolts in sensor circuits to hundreds of kilovolts in power transmission networks.
In direct current (DC) systems, voltage describes a constant potential difference between two points, while in alternating current (AC) systems, both the root mean square (RMS) value and the waveform over time are considered. For electronic devices, voltage determines not only proper operation but also operational safety. As a measurement unit, the volt is widely used in testing instruments, technical documentation, and international standard systems.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.