+15,00,000 products in offer
7,000 packages per day
+3,00,000 clients from 150 countries
Gyroscope is a device used to measure and maintain the spatial orientation of an object based on the principle of conservation of angular momentum. A traditional mechanical gyroscope consists of a rapidly spinning rotor mounted within a frame that allows free rotation around one or more axes. When the rotor is in motion, its axis of rotation maintains a constant orientation relative to inertial space, which makes it possible to detect changes in the orientation of the device with respect to that reference.
The stability of the gyroscope’s spin axis is a result of physical laws governing moment of inertia and forces acting on rotating bodies. When an attempt is made to change the rotor’s orientation, the resulting precession effect forms the basis for the gyroscope’s operation in navigation and stabilization systems. Modern applications of gyroscopes span a wide range of fields—from aviation and marine or satellite navigation to consumer technologies such as smartphones, drones, and gaming consoles.
With technological advancement, new types of gyroscopes have emerged that do not rely on mechanical components. Fiber-optic gyroscopes (FOG) and gyroscopes based on light wave or solid-body vibration interference (MEMS – Micro-Electro-Mechanical Systems) enable miniaturization and deployment in applications requiring high precision and resistance to mechanical disturbances. MEMS gyroscopes have become particularly widespread due to their low cost and compact size, allowing integration with other sensors in Inertial Measurement Units (IMUs).
Regardless of the underlying technology, the core function of a gyroscope remains the measurement of angular velocity, which enables tracking spatial position changes and movement direction. Such data are essential in autonomous systems, robotics, image stabilization, missile guidance, and vehicle motion compensation. Due to their ability to operate independently of external signals, gyroscopes are a critical component of inertial navigation systems.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.