+15,00,000 products in offer
7,000 packages per day
+3,00,000 clients from 150 countries
Date of publication: 31-12-2024 Update date: 10-04-2026 🕒 4 min read
Step by step we will show you how to quickly build a simple, mobile robot based on the POLOLU Romi chassis. But that's not all, in the next guide we will show you what you can use this construction for.
The Romi chassis is a small, round robot base that moves on two wheels. It comes with a spot for six AA batteries and has an option to add a small ball at the front for balance. You can attach various electronic parts like controllers and sensors.
The chassis is versatile and comes in different colours, making it great for many robot projects.
You can power the chassis in different ways:
The Romi chassis has many holes and slots of different sizes. These make it easy to attach extra parts and customise your robot. You can use different screws and standoffs to secure additional components like sensors, cameras, or extra circuit boards.
After putting the chassis together and setting up the power, you can add and program the electronics to control your robot. The Romi 32U4 Control Board and other optional parts can help you create a fully functioning robot. You can program the robot to perform various tasks, like navigating obstacles, following lines, or responding to sensors.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.