+15,00,000 products in offer

7,000 packages per day

+3,00,000 clients from 150 countries

Quick Buy Favourites
Cart

AUX - definition

AUX (eng. Auxiliary) is a term used in consumer electronics and audio systems as an abbreviation for the word auxiliary, meaning a supplementary or additional function. It most commonly refers to an audio input or output that allows an external sound source to be connected to an amplifier, speaker set, car radio, or other sound playback device.

The AUX input is typically implemented in the form of a 3.5 mm jack or RCA socket, and its primary feature is the analog nature of signal transmission. It allows for the transmission of uncompressed audio signals directly from the headphone output of a phone, MP3 player, computer, or other source, without the need for digital processing. In practice, this means ease of use and wide compatibility with many devices.

Due to the unspecified input signal voltage level, the sound quality in an AUX connection may depend on the impedance characteristics of the source and receiver, as well as the quality of the cable used. The lack of standardization of signal parameters makes AUX a universal solution, but with limited resistance to interference and signal loss over long cables.

In modern electronic systems, the AUX function is sometimes replaced by digital interfaces, such as Bluetooth or USB, but it still remains a commonly used and simple way to connect audio devices in consumer and industrial applications.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO