+13,00,000 products in offer
7,000 packages per day
+3,00,000 clients from 150 countries
An Electrode is a conductive component of an electrochemical system that allows an electrical charge to flow between an external circuit and an electrolyte, acting as an interface between an electron and an ionic conductor. Depending on the direction of current flow and the type of redox reactions taking place, the electrode can act as anode or cathode. Its primary function is to initiate and sustain electrochemical reactions by exchanging electrons with ions present in solution.
In galvanic cells electrodes participate in spontaneous chemical reactions generating a voltage, while in electrolytic systems they enable the reaction to be forced by an external current source. The oxidation or reduction of chemicals takes place at the electrodes, accompanied by electron transfer between the electrode and the molecules in the electrolyte.
The electrode material must have good electrical conductivity, chemical and electrochemical resistance and stability under the operating conditions of the system. Typical electrode materials include metals, graphite, alloys, as well as conductive oxides and composite materials. In specialised applications, reference electrodes of known potential are also used to calibrate and measure electrochemical voltage.
Electrodes are an indispensable component in technologies such as electrochemical cells, rechargeable batteries, electrodes in welding machines, measurement electrodes in sensors, and in medicine, where they are used in diagnostics and therapy, e.g. in electrocardiography or neuromuscular stimulation. The design and properties of electrodes have a direct impact on the efficiency, selectivity and durability of the systems in which they are used.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.