+15,00,000 products in offer
7,000 packages per day
+3,00,000 clients from 150 countries
An Electrolyte is a substance capable of conducting electricity due to the presence of free ions. Unlike electron conductors such as metals, conductivity in electrolytes occurs due to the movement of positive and negative ions in solution or solid phase. Electrolytes can take the form of liquids, solids or gels and play a key role in electrochemical processes such as electrolysis, the operation of galvanic cells or the functioning of Rechargeable Batteries.
Chemically, electrolytes are divided into strong and weak electrolytes, depending on their degree of dissociation in solution. Strong electrolytes dissociate completely into ions, giving them high conductivity, while weak electrolytes dissociate only partially. Typical examples are acids, bases and salts dissolved in water, but also solids such as certain oxides and ion-conducting glasses can act as an electrolyte, especially in modern lithium Batteries.
In an electrochemical system, the electrolyte allows ions to flow between electrodes, providing closure of the electrical circuit and conditions for redox reactions. Its properties - such as ionic conductivity, chemical stability, viscosity, operating temperature range or compatibility with electrode materials - have a direct impact on the efficiency and durability of the system.
Electrolyte selection is crucial in the design of electrochemical devices. In Rechargeable Batteries, it determines the nominal voltage, capacity, charging time and safety of use. In chemical sensors, the electrolyte influences the sensitivity and selectivity of the measurement, while in electrochemistry industrial it influences the efficiency of the electrolytic processes and the purity of the resulting products. Many modern applications also make use of solid or polymer electrolytes, which combine mechanical properties with an ion-conducting function, offering new design and technological possibilities.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.