+13,00,000 products in offer

7,000 packages per day

+3,00,000 clients from 150 countries

Quick Buy Favourites
Cart

Filter - definition

A Filter is a circuit or algorithm for the selective processing of physical signals, in particular electrical, acoustic or digital signals, in order to amplify desired components and suppress undesired ones. The operation of a filter involves modifying the frequency spectrum of a signal to control its energy properties, temporal or spectral structure. Filters are a key component in communication, electronic, control, measurement and multimedia systems.

From the point of view of signal theory, a filter implements a specific transition function that describes the response of the system to the different frequency components of the input signal. Depending on the characteristics of this function, filters are divided into low-pass, high-pass, band-pass and band-stop filters. Each of these types allows the selection of a specific frequency range, which is necessary for noise suppression, signal separation or system response formation.

Filters can be implemented in analogue or digital form. Analogue filters use passive elements (resistors, capacitors, coils) and/or active elements (operational amplifiers) to modify the signal in real time. Digital filters process numerically sampled signals, allowing great flexibility in the design and adaptation of frequency characteristics. Their implementation is done using numerical algorithms and DSPs or microcontrollers.

In real systems, filters can also perform protection (e.g. surge suppression), conditioning (e.g. waveform smoothing), and diagnostic functions (e.g. noise signal extraction). In advanced applications, adaptive, non-linear, time-varying and spatial filters are used, depending on the nature of the signal and application requirements. Their effectiveness is assessed by parameters such as attenuation, selectivity, slope, stability and phase distortion.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO