+15,00,000 products in offer
7,000 packages per day
+3,00,000 clients from 150 countries
Electric current density is a physical quantity that describes the distribution of current with respect to the cross-section of a conductor. It is expressed as the ratio of the electric current flowing through a given area to the area of that cross-section. Its unit in the SI system is the ampere per square metre (A/m²). Current density is a vector, which means that it has both a value and a direction - in line with the direction of positive charge flow.
In technical and engineering applications, this concept plays an important role in the design of conductors, semiconductor components and electrotechnical devices. It allows an assessment to be made as to whether a particular design provides safe and efficient conditions for current flow without the risk of overheating, excessive energy loss or damage to the conductive material. Too high a current density can lead to localised temperature rises, electromigration phenomena, as well as damage insulation or component degradation.
In homogeneous and linearly conducting materials, the current density depends on the electric field according to Ohm's law in local form. In inhomogeneous or microscale structures, the current density distribution can be non-uniform, requiring analysis using numerical methods. In microelectronics and thin-film technology, precise control of this quantity is crucial to ensure the reliability and longevity of circuits.
In circuit analysis and electromagnetic field theory, current density is also relevant to Maxwell's equations, which describe the relationships between electric, magnetic fields and the distribution of currents in a medium.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.