+15,00,000 products in offer

7,000 packages per day

+3,00,000 clients from 150 countries

Quick Buy Favourites
Cart

HVAC - definition

HVAC (Heating, Ventilation, and Air Conditioning) is a collection of technologies and engineering systems used to control air performance in buildings and confined spaces, including heating, ventilation and air conditioning. Its purpose is to ensure optimal thermal conditions and indoor air quality, which is crucial for occupant comfort, energy efficiency and meeting environmental and sanitary standards.

HVAC systems integrate thermodynamic, mechanical and Automation control systems to precisely manage heat exchange, humidity and air filtration. Heating technology uses heat sources such as gas boilers, heat pumps, resistance systems and energy recovery technologies where waste heat is used to improve the energy balance of the building. Ventilation provides air exchange through mechanical, natural or hybrid systems, using recuperation and dynamic flow control to minimise heat loss and optimise energy consumption.

Air-conditioning systems operate using compressor, absorption and adiabatic cooling systems, controlling temperature and humidity levels. Advanced refrigerants with low greenhouse effect potential are used, and adaptive control systems use predictive and sensory algorithms that dynamically adjust the system's operating parameters depending on the heat load and external conditions.

The integrated control of HVAC systems is implemented by BMS (Building Management System) systems that monitor and optimise the operation of components in real time, using IoT and artificial intelligence technologies to analyse energy consumption and forecast changes in weather conditions. The implementation of energy management strategies includes the use of heat and cold storage, passive thermal control systems and intelligent airflow control systems to provide increased operational efficiency and minimise environmental impact.

HVAC standards and regulations are defined by international standards such as ASHRAE, ISO 16890 and EN 13779, specifying requirements for energy efficiency, filtration and acceptable indoor air quality parameters. HVAC technologies are used in residential, commercial and industrial buildings, with developments focused on automation, minimising energy losses and implementing net-zero emission solutions in line with sustainable development and smart city policies.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO