+13,00,000 products in offer

7,000 packages per day

+3,00,000 clients from 150 countries

Quick Buy Favourites
Cart

I²C - definition

I²C (Inter-Integrated Circuit) is a synchronous serial communication bus designed by Philips (now NXP Semiconductors) to enable data exchange between integrated circuits over short distances. The I²C bus consists of two lines: SDA (data) and SCL (clock), which are common to all devices connected to the bus and operate in open drain mode, enabling multi-module communication and the use of multiple master and slave devices.

Communication follows an established frame protocol, which includes device addressing, transmission acknowledgement (ACK/NACK) and data transfer in both directions. Each slave device is identified by a unique address, allowing multiple systems to operate simultaneously on a single bus. Logic signals are transmitted using voltages compatible with TTL or CMOS levels, and transmission speeds can range from the standard 100 kbps to several megabits per second in fast and extended modes.

The advantage of I²C is the simplicity of implementation and the economy of signal lines, which makes this bus widely used in embedded devices, microcontrollers, sensors, EEPROMs, RTC clocks or Displays. With the ability to easily add additional components without modifying the main controller, I²C facilitates the integration and prototyping of electronic systems. However, due to the characteristic limitations of the bus - such as cable length, line capacitance and noise immunity - I²C is mainly used in systems on a single board or within a single device.

The I²C standard is open and widely adopted in industrial and consumer electronic systems. Its popularity is due to its high flexibility, compatibility with a wide range of devices and availability in almost all modern microcontrollers.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO