+15,00,000 products in offer
7,000 packages per day
+3,00,000 clients from 150 countries
Electric induction is a physical phenomenon involving the generation of an electric charge or potential difference (voltage) under the action of an alternating magnetic field or the presence of an external electric charge. The term is sometimes used in two main contexts: as electrostatic induction and as electromagnetic induction, both cases describing different mechanisms for generating electrical phenomena.
In the case of electromagnetic induction, described by Faraday's law, a time-varying magnetic field crossing an electrical circuit produces an electromotive force, which can induce current flow. This is the basic mechanism of operation of generators, transformers and induction coils and is the foundation of electric power technology. The magnitude of the induced electromotive force depends on the rate of change of magnetic flux and the number of turns in the circuit.
Electrostatic induction, on the other hand, involves the displacement of free charges in a conductor as a result of an external electric field. When an electrified body approaches a conductor, there is a separation of charges within the material - some are attracted, others repelled - leading to local potential differences. This phenomenon is used in capacitors, electrostatic shielding and non-contact object detection devices.
From a physical point of view, electrical induction is a consequence of the interactions between charges and fields and a means of energy transfer in dynamic systems. The mathematical description uses integral and differential forms of Maxwell's equations, which precisely describe the relationships between field strength, potential and induced electrical phenomena. Induction is a key element in many technological phenomena and underpins the operation of numerous electronic and electromechanical components.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.