+15,00,000 products in offer

7,000 packages per day

+3,00,000 clients from 150 countries

Quick Buy Favourites
Cart

Lossless compression - definition

Lossless compression is a method of encoding data that makes it possible to reduce its volume while maintaining the full integrity of the information. This means that after decompression it is possible to accurately reconstruct the original data bit by bit, without any loss of content. The process is based on identifying and eliminating redundancies - that is, repeated sequences, patterns or symbols - while using efficient coding methods to represent this information in a more compact way.

Lossless compression is used wherever full data fidelity is important, e.g. in text documents, source code, binary archives, medical images, databases or in data transmission between computer systems and measurement devices. In audio and video systems, it can also be used, especially in professional applications where any distortion of the source signal is unacceptable.

Others use various lossless compression algorithms in engineering practice, the most popular of which are Huffman, LZW (Lempel-Ziv-Welch), DEFLATE, Burrows-Wheeler or predictive algorithms used e.g. in PNG, FLAC or ZIP formats. Their effectiveness depends on the structure of the input data - the greater the repeatability and predictability of the data, the higher the possible compression ratio. In contrast to lossy methods, lossless compression does not introduce artefacts and does not change the characteristics of the signal, making it ideal for archiving, transmission of critical data and for scientific and engineering purposes.

Algorithms of this type must strike a balance between compression rate, processing time and computational complexity. Systems with limited computing power or memory use simplified versions of compression that guarantee fast performance with an acceptable level of data reduction. In the context of embedded systems, Automation and IoT devices, lossless compression plays a key role in efficiently transferring and storing data while keeping its content intact.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO