+15,00,000 products in offer
7,000 packages per day
+3,00,000 clients from 150 countries
Electric power is a physical quantity describing the rate at which electrical energy is transferred, consumed or transformed into another form of energy, e.g. heat, mechanical or light. In electrical systems, power is expressed in watts (W) and is the product of voltage and current. In the case of direct current, the calculation is unambiguous, whereas for alternating current (AC)the phase relationship between voltage and current must be taken into account, which leads to a distinction between active, reactive and apparent power.
Active power (P) represents the actual energy transferred to the load and transformed into useful work or heat. Reactive power (Q) is related to the transfer of energy between the Inductive Components and Capacitive Components of a circuit, which do not do useful work but affect the operating conditions of the network. Apparent power (S) is the geometric sum of active and reactive power, expressed in volt-amperes (VA), and describes the total flow of energy in a circuit.
Also important in the analysis of electrical power is the concept of power factor (cos φ), which describes the ratio of active to apparent power and is a measure of the efficiency of energy use in a circuit. In engineering practice, the aim is to maximise this ratio in order to reduce energy losses and improve the stability of the power supply network.
Understanding electrical power is crucial in the design and operation of equipment and electrical systems. It allows for the proper selection of protection, Cables, power sources and controls, and enables the assessment of the energy efficiency of systems. In large-scale power systems, such as transmission networks, power management is strategic, affecting the energy balance and reliability of supply.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.