+15,00,000 products in offer

7,000 packages per day

+3,00,000 clients from 150 countries

Quick Buy Favourites
Cart

Rated power - definition

Power rating is the maximum value, as specified by the manufacturer, of the power that an electrical, electronic or mechanical device can permanently give out, consume or process in a safe and compatible manner for its intended use, while maintaining its nominal operating parameters. It is the value determined under laboratory or reference conditions, such as ambient temperature, supply voltage, frequency or cooling level, which comply with the technical standards for the type of device.

Rated power is an important criterion for assessing the operating capability of a device and its selection for a specific application. For loads such as Electric Motors, heaters, transformers or Power Supplies, it determines the operating level at which both efficiency and operating life are ensured. Exceeding this value can lead to overheating, overloading, reduced efficiency and, in extreme cases, damage or destruction of the equipment.

In the case of Power Sources, such as generators, photovoltaic panels or audio amplifiers, power rating refers to the maximum energy they can deliver continuously without risking degradation of their performance. In practice, the concept of instantaneous or peak power may also be used, referring to a brief overload that does not adversely affect the life of the system - but it is the rated power that remains the primary reference parameter.

The indication of the rated power on equipment nameplates and in the technical documentation enables its correct use and integration with other system components, ensuring safety and compliance with installation requirements.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO