+15,00,000 products in offer

7,000 packages per day

+3,00,000 clients from 150 countries

Quick Buy Favourites
Cart

Safe area of work (SOA) - definition

Safe Operating Area (SOA) is a defined range of operating parameters of an electronic device, in particular semiconductor power components such as transistors, Thyristors or Diodes, within which the device can operate without risk of thermal damage, breakdown or overload. The SOA characteristic defines the limits of permissible values of voltage, current and duration of pulses, within which the component retains its full functionality and operational life.

The SOA is usually represented in the form of a graph in a voltage-current coordinate system in which various constraints, such as maximum collector-emitter voltage, maximum collector current, loss power limits and secondary effect constraints (e.g. avalanche effect or secondary emission electrons), define the limits of safe device operation. Exceeding any of these limits can lead to destruction of the Semiconductor structure due to overheating, dynamic overload or mechanical damage to the junction area.

Analysis and adherence to SOA boundaries is crucial in the design of high reliability systems such as power converters, high-end audio amplifiers, drive systems and emergency power systems. In pulsed applications, a pulsed Reverse Bias Safe Operating Area (RBSOA) is additionally defined, which takes into account the dynamic switching conditions of the Transistors, important to minimise switching losses and ensure the long-term reliability of electronic devices.

In modern IGBT transistors, MOSFETs or SiCs, the SOA is optimised through advanced Semiconductor structure engineering techniques such as doping grading, the use of buffer layers and specialised channel profiles to increase the component's resistance to extreme operating conditions and improve its thermal characteristics.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO