+15,00,000 products in offer

7,000 packages per day

+3,00,000 clients from 150 countries

Quick Buy Favourites
Cart

Crowbar circuit - definition

A crowbar circuit is a protection circuit used in electronic and power systems to quickly and effectively reduce the output voltage to a very low level (close to zero) in the event of its uncontrolled rise above an acceptable threshold value. The crowbar works by shorting the power line to ground or the negative rail with a conductive element, most commonly a Thyristors, Triacs or Transistors, resulting in the blowing of a fuse or the tripping of another mechanism to cut off the power supply.

This circuit does not regulate the voltage continuously, but acts as a fail-safe, activated immediately when a predetermined threshold is exceeded. It is often used in stabilised power supplies, power supply systems for sensitive digital circuits, and telecommunications and industrial equipment where over-voltage could lead to permanent component damage. Comparators, Zener diodes or other voltage reference circuits are used to detect abnormal voltages and control the execution element of the crowbar.

A typical crowbar circuit operates quickly and reliably, providing protection even in the event of sudden surges. It has the advantage of simplicity of design and no need for continuous monitoring of the power condition on the receiving side, as the response is automatic. In design practice, however, the effect of the crowbar on the load and the power source must be taken into account, as its tripping involves the momentary flow of large short-circuit currents. This requires appropriate selection of protective components, including fuses or automatic power disconnection systems.

This type of circuit is also used in more advanced overvoltage protection systems, as a supplement to clamp type circuits that limit the voltage instead of short-circuiting it. Despite the development of modern protection methods, the crowbar remains an effective and reliable solution in many industrial and laboratory applications.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO