+15,00,000 products in offer
7,000 packages per day
+3,00,000 clients from 150 countries
Radar (Radio Detection and Ranging) is a remote object detection and location system based on the emission and reception of radio waves. It works by sending electromagnetic pulses in the direction of the observed space and then analysing the signals reflected from the obstacles encountered. On the basis of the wave return time and its characteristics, it is possible to determine the distance, speed, angular position and sometimes the structure of a detected object.
Radar uses the physical phenomena associated with the propagation of electromagnetic waves, including reflection, refraction and scattering. Emission is typically realised by a transmitting antenna that generates a beam at a specific frequency. The reflected signals are then captured by the receiving antenna and processed using detection circuits, amplifiers and digital systems, often supported by algorithms filtering and analysis.
Radar systems operate over a wide range of radio frequencies, from metre to millimetre bands, allowing them to be adapted to different operational conditions. There are many types of radar, including pulsed, continuous, Doppler, fusion data and imaging, each with specific applications and characteristics.
Applications of radar include aviation, shipping, automotive, meteorology, air traffic control, satellite observations, military systems and autonomous mobile systems. In meteorology, radar enables precipitation detection and analysis of atmospheric dynamics, while in aviation it is used for collision avoidance and navigation. In military applications, it plays a role in early warning, target detection and fire control.
Advanced radar systems use the techniques of digital signal processing, beamforming and tracking multiple targets simultaneously. The effectiveness of radar depends on parameters such as transmitter power, receiver sensitivity, wavelength, antenna characteristics and the level of environmental interference.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.