+15,00,000 products in offer
7,000 packages per day
+3,00,000 clients from 150 countries
Heatsinks are passive cooling system components used to efficiently dissipate heat generated by electronic, electrical and mechanical devices in order to maintain optimal operating conditions and prevent overheating. Its operation is based on thermal conductivity and convection, which enable the transfer of heat energy from the surface of the heat-emitting component to the environment. The high thermal conductivity of the material and the optimised geometry of the Heatsinks structure determine its effectiveness in the thermal exchange process.
Heatsinks consist of a body made of metals with high thermal conductivity, usually aluminium or copper, and a fin structure that increases the heat emission surface area. The geometry of the fins can be tailored to the type of cooling - passive systems use Heatsinks with a large air contact area, while active systems working with fans or coolant systems use designs optimised to maximise thermal flow and minimise aerodynamic drag.
Heatsinks are used in power, semiconductor and power systems where effective thermal loss management is key. In electronics, Heatsinks are integral to the cooling of processors, power Transistors, amplifiers and LED modules, ensuring stable performance under high heat loads. In industrial systems, dedicated designs are used to cool power converters, transformers and power electronics systems, where the efficiency of thermal exchange has a direct impact on system reliability.
Heatsinks' efficiency depends on the thermal conductivity coefficient of the material, its mass and the way it is mounted on the surface of the heat transfer element. The use of Thermoconductive pastes, Thermoconductive tapes and Heat conductive compounds minimises the thermal resistance at the surface interface, which increases the efficiency of energy dissipation. Heatsinks combining natural and forced convection are used in applications with increased cooling requirements, while high-power systems implement liquid-cooled systems and the use of heat chambers and heat pipes to further assist in the transport of heat over a distance.
Heatsinks materials are subjected to surface treatments such as anodising or powder coating to improve resistance to corrosion and affect thermal emission characteristics. For applications requiring weight minimisation, lightweight alloy composite materials are used, providing an optimum ratio of weight to cooling efficiency. Dynamic analysis of heat transfer in Heatsinks takes into account the effects of thermal radiation, airflow turbulence and local temperature gradients, which is crucial in the precise design of cooling systems for applications requiring high reliability and operational stability.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.